Porting from MPC8248 to LS1020A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Porting from MPC8248 to LS1020A

跳至解决方案
3,226 次查看
victormazin
Contributor II

Hi

Our task is to port the Linux operation system and set of servers and drivers (written in C language) from Freescale MPC8248 processor to Freescale LS1020A processor.

Which first steps could you recommend to us?

Regards

Victor

标签 (1)
0 项奖励
回复
1 解答
3,024 次查看
lunminliang
NXP Employee
NXP Employee

Hello Victor Mazin,

If you are using new platform other than LS1021ATWR, as Alexander has suggested, you're recommend to porting from Freescale QorIQ SDK, since it has already included support for LS1021A.

Some steps of porting u-boot including creating configuration file based on ls1021atwr.h, ls1021atwr.c, ddr.c, ls1_rcw.cfg, ls1_pbi.cfg and rebuilding images, porting Linux including creating new file based on mach-ls1021a.c, ls1021a_defconfig, new device tree, and so on. There is application note of U-Boot and Linux porting on T4240 system, although it's not for LS1021A I think it may be also helpful.

http://cache.freescale.com/files/32bit/doc/app_note/AN4814.pdf?fsrch=1&sr=1&pageNum=1


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,025 次查看
lunminliang
NXP Employee
NXP Employee

Hello Victor Mazin,

If you are using new platform other than LS1021ATWR, as Alexander has suggested, you're recommend to porting from Freescale QorIQ SDK, since it has already included support for LS1021A.

Some steps of porting u-boot including creating configuration file based on ls1021atwr.h, ls1021atwr.c, ddr.c, ls1_rcw.cfg, ls1_pbi.cfg and rebuilding images, porting Linux including creating new file based on mach-ls1021a.c, ls1021a_defconfig, new device tree, and so on. There is application note of U-Boot and Linux porting on T4240 system, although it's not for LS1021A I think it may be also helpful.

http://cache.freescale.com/files/32bit/doc/app_note/AN4814.pdf?fsrch=1&sr=1&pageNum=1


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,025 次查看
victormazin
Contributor II

Thank you Lunmin and Alexander,

We will try to following your recommendations

Regards

Victor.

0 项奖励
回复
3,025 次查看
alexander_yakov
NXP Employee
NXP Employee

We do not offer porting guide for this case.

I recommend building a new Linux from our Linux SDK we offer for LS1020A processor, and than port your applications from MPC8248 to LS1020A using build tools supplied in our Linux SDK.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复