Porting from MPC8248 to LS1020A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting from MPC8248 to LS1020A

ソリューションへジャンプ
3,220件の閲覧回数
victormazin
Contributor II

Hi

Our task is to port the Linux operation system and set of servers and drivers (written in C language) from Freescale MPC8248 processor to Freescale LS1020A processor.

Which first steps could you recommend to us?

Regards

Victor

ラベル(1)
0 件の賞賛
返信
1 解決策
3,018件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Victor Mazin,

If you are using new platform other than LS1021ATWR, as Alexander has suggested, you're recommend to porting from Freescale QorIQ SDK, since it has already included support for LS1021A.

Some steps of porting u-boot including creating configuration file based on ls1021atwr.h, ls1021atwr.c, ddr.c, ls1_rcw.cfg, ls1_pbi.cfg and rebuilding images, porting Linux including creating new file based on mach-ls1021a.c, ls1021a_defconfig, new device tree, and so on. There is application note of U-Boot and Linux porting on T4240 system, although it's not for LS1021A I think it may be also helpful.

http://cache.freescale.com/files/32bit/doc/app_note/AN4814.pdf?fsrch=1&sr=1&pageNum=1


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,019件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Victor Mazin,

If you are using new platform other than LS1021ATWR, as Alexander has suggested, you're recommend to porting from Freescale QorIQ SDK, since it has already included support for LS1021A.

Some steps of porting u-boot including creating configuration file based on ls1021atwr.h, ls1021atwr.c, ddr.c, ls1_rcw.cfg, ls1_pbi.cfg and rebuilding images, porting Linux including creating new file based on mach-ls1021a.c, ls1021a_defconfig, new device tree, and so on. There is application note of U-Boot and Linux porting on T4240 system, although it's not for LS1021A I think it may be also helpful.

http://cache.freescale.com/files/32bit/doc/app_note/AN4814.pdf?fsrch=1&sr=1&pageNum=1


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,019件の閲覧回数
victormazin
Contributor II

Thank you Lunmin and Alexander,

We will try to following your recommendations

Regards

Victor.

0 件の賞賛
返信
3,019件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

We do not offer porting guide for this case.

I recommend building a new Linux from our Linux SDK we offer for LS1020A processor, and than port your applications from MPC8248 to LS1020A using build tools supplied in our Linux SDK.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信