Packrfs failed? ubuntu is incomplete

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Packrfs failed? ubuntu is incomplete

ソリューションへジャンプ
2,234件の閲覧回数
m_kei
Contributor III

I am trying to generate RFS in LSDK2108. We are trying to build userland by referring to "How to build various userland with custom packages" in the LSDK2108 user guide.

Whenever I run "flex-builder -i packrfs", I get something like the following error message.

/xxx/flexbuild_lsdk2108/build/rfs/rootfs_lsdk2108_ubuntu_main_arm64 is incomplete

Since no further messages are output, it is difficult to tell if this is an error or not. What kind of output message is this?

Is it an error? Or is it an advice to continue doing mkboot?

 

0 件の賞賛
返信
1 解決策
2,230件の閲覧回数
m_kei
Contributor III

The cause seems to have been a corrupted file in build/rfs or some other problem.

For some reason, build/rfs was not erased even with cleanrfs, and because of the corrupted rfs file, the rootfs is not created in mkrfs, resulting in an error that there is no target rootfs as packrfs.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,622件の閲覧回数
mdecandia
Contributor III

Hi all,

which is the cause and the solution for this kind of error?

0 件の賞賛
返信
2,231件の閲覧回数
m_kei
Contributor III

The cause seems to have been a corrupted file in build/rfs or some other problem.

For some reason, build/rfs was not erased even with cleanrfs, and because of the corrupted rfs file, the rootfs is not created in mkrfs, resulting in an error that there is no target rootfs as packrfs.

0 件の賞賛
返信
2,231件の閲覧回数
m_kei
Contributor III

The packrfs command is supposed to generate rootfs, but when this error is printed, rootfs was not generated in the image folder. In other words, packrfs has failed.

However, as shown above, it only shows "incomplete", so it is unclear why it is failing. What is the cause of the error?

0 件の賞賛
返信