PCIe loopback test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe loopback test

3,445 Views
srinivas_hk
Contributor I

We are using LS1046A in our design. We have PCIe X2 lane and PCIe X1 lane both configured at Gen3. This is RC and the EP is Qualcomm device. I would like to run pcie loopback test between RC (LS1046A) and QCA device. to verify the overall throughput.

I got a sequence of commands that we have to execute to create a loopback from RC. I am able to confirm that loopback is created post reading the status. Now i would like to run pcie test. How to do that ??

Please suggest

0 Kudos
Reply
2 Replies

3,353 Views
srinivas_hk
Contributor I

Basically read write stress test between RC and EP. It can be a prbs pattern or some pattern which gets transmitted from RC  and when received it should match.

0 Kudos
Reply

3,353 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> Now i would like to run pcie test.

Which exactly test you want to run?

0 Kudos
Reply