PCIe hotplug support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,760件の閲覧回数
TrinathK
Contributor III

Hi

I have a PCIe communication between ls1043ardb (layerscape board as Root complex) and Beagleboard x15 (as endpoint). I enabled PCIe hotplug in kernel configuration of ls1043ardb.

And i have already used "remove" and "rescan" and everything is working fine. I can able to detect my endpoint after rescan. but sometimes BARs are not being assigned.

Firstly, how may i know if a board support hotplug feature or not. In reference manual of ls1043 and ls1046, nothing is mentioned about pcie hotplug. Does ls1043 and ls1046 support hotplug feature ?

Also as per my understanding, hardware support is also required for hotplug feature to work. please explain on it.

Thanks in advance.

0 件の賞賛
返信
1 解決策
2,753件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Does ls1043 and ls1046 support hotplug feature ?

The processors do not support Hot-Plug.

References:

QorIQ LS1043A Reference Manual, 28.4.2.45.2 Function

LS1046A Reference Manual, 25.4.2.60.2 Function

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,754件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Does ls1043 and ls1046 support hotplug feature ?

The processors do not support Hot-Plug.

References:

QorIQ LS1043A Reference Manual, 28.4.2.45.2 Function

LS1046A Reference Manual, 25.4.2.60.2 Function

0 件の賞賛
返信