PCIe hotplug support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCIe hotplug support

跳至解决方案
2,744 次查看
TrinathK
Contributor III

Hi

I have a PCIe communication between ls1043ardb (layerscape board as Root complex) and Beagleboard x15 (as endpoint). I enabled PCIe hotplug in kernel configuration of ls1043ardb.

And i have already used "remove" and "rescan" and everything is working fine. I can able to detect my endpoint after rescan. but sometimes BARs are not being assigned.

Firstly, how may i know if a board support hotplug feature or not. In reference manual of ls1043 and ls1046, nothing is mentioned about pcie hotplug. Does ls1043 and ls1046 support hotplug feature ?

Also as per my understanding, hardware support is also required for hotplug feature to work. please explain on it.

Thanks in advance.

0 项奖励
回复
1 解答
2,737 次查看
ufedor
NXP Employee
NXP Employee

> Does ls1043 and ls1046 support hotplug feature ?

The processors do not support Hot-Plug.

References:

QorIQ LS1043A Reference Manual, 28.4.2.45.2 Function

LS1046A Reference Manual, 25.4.2.60.2 Function

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,738 次查看
ufedor
NXP Employee
NXP Employee

> Does ls1043 and ls1046 support hotplug feature ?

The processors do not support Hot-Plug.

References:

QorIQ LS1043A Reference Manual, 28.4.2.45.2 Function

LS1046A Reference Manual, 25.4.2.60.2 Function

0 项奖励
回复