PCIe data transfer rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe data transfer rate

3,625件の閲覧回数
SrinivasP
Contributor II

I want to get clarified on PCIe transfer rate (or Baud rate) in LS1043A I.MX8Q. As per PCIe spec and generation a specified transfer rate is mentioned (2. GTps , 5 GTps etc). Is this transfer rate fixed or can we configure any transfer rate below the maximum specified  rate.

0 件の賞賛
返信
2 返答(返信)

3,617件の閲覧回数
SrinivasP
Contributor II

Thank you for the reply. As I understand (If I am not wrong) , you mean that the data (Packet) is transferred over the PCIe link at a rate of of 2.5 GTps or 5 or 8 GTps (based on PCIe generation). 

If my understanding is right, can be use cables from one backplane to other , to transfer data over PCIe at this rate. Are there any specialized cables for this purpose.

0 件の賞賛
返信

3,620件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is this transfer rate fixed

The PCIe link rate is fixed.

Consider that data is transferred through this link in packets, so resulting data rate can vary.