PCIe Switch with NTB for LS1043RDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCIe Switch with NTB for LS1043RDB

3,052 次查看
SrinivasP
Contributor II

Hi,

We recently purchased LS1043ARDB and we have a requirement to perform I/O interfaces through  a PCIe switch (at least two end points). Please suggest a suitable PCIe switch (with one NTB port) compatible to LS1043ARDB and has linux drivers availability.

Thanks in advance.

Srinivas P

0 项奖励
回复
2 回复数

3,048 次查看
ufedor
NXP Employee
NXP Employee

The LS1043A PCI Express interface is compatible with the PCI Express™ Base Specification, Revision 3.0 definition, architecture and implementation. This means that any compatible PCIe switch can be connected to the LS1043ARDB.

NXP provides Linux SDK for Layerscape processors, the switch manufacturer should provide driver for the product.

0 项奖励
回复

3,046 次查看
SrinivasP
Contributor II

Thank you

0 项奖励
回复