PCIe Switch with NTB for LS1043RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe Switch with NTB for LS1043RDB

3,023 Views
SrinivasP
Contributor II

Hi,

We recently purchased LS1043ARDB and we have a requirement to perform I/O interfaces through  a PCIe switch (at least two end points). Please suggest a suitable PCIe switch (with one NTB port) compatible to LS1043ARDB and has linux drivers availability.

Thanks in advance.

Srinivas P

0 Kudos
Reply
2 Replies

3,019 Views
ufedor
NXP Employee
NXP Employee

The LS1043A PCI Express interface is compatible with the PCI Express™ Base Specification, Revision 3.0 definition, architecture and implementation. This means that any compatible PCIe switch can be connected to the LS1043ARDB.

NXP provides Linux SDK for Layerscape processors, the switch manufacturer should provide driver for the product.

0 Kudos
Reply

3,017 Views
SrinivasP
Contributor II

Thank you

0 Kudos
Reply