Official performance data about LS1043A's Max. throughput

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Official performance data about LS1043A's Max. throughput

1,727 Views
彥圻沈
Contributor I

We plan to use LS1043A as a 802.11ac AP and hope it can cover 802.11ax. Is there any official performance data ? 

0 Kudos
Reply
2 Replies

1,624 Views
彥圻沈
Contributor I

Hi Yiping

     do you have the information about test structure ? it is only Ethernet to Ethernet or Ethernet-Wireless to Wireless-Ethernet? 

0 Kudos
Reply

1,624 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello 彥圻 沈,

Please refer to the following IPv4 forward 4 cores 6G test result in Linux SDK 1809 test with Linux Kernel 4.14 on LS1043ARDB.

FrameSize(Byptes)              Throughput(%)

64                                           9.37

128                                         18.05

256                                          24.98

390                                          48.0

512                                           56.2

1024                                         100.0

1280                                         100.0

1518                                         100.0


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply