OTP on Layerscape

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OTP on Layerscape

2,866 次查看
mrmichaelt86
Contributor I

Hello.  Is there any sort of serial number or ID marked in the layerscape di?  Apart from Zone-of-Trust HSK, is there any ability to set an identifying serial number per device?  I would simply like to read a number in U-Boot and pass it to the Linux application, which is a unique number identifying the device.  If necessary, I will use the Security Secret Key, but exposing this in Linux Configuration space would be a security risk

0 项奖励
回复
4 回复数

2,656 次查看
guignbt2v
Contributor III

Hi. Is there something similar for the LX2160?

0 项奖励
回复

2,859 次查看
ufedor
NXP Employee
NXP Employee

Which exactly processor is in question?

0 项奖励
回复

2,842 次查看
mrmichaelt86
Contributor I

Processor in Question:  LS1046A

0 项奖励
回复

2,837 次查看
ufedor
NXP Employee
NXP Employee

Security fuse processor (SFP) contains 64-bit Factory Unique ID in two 32-bit registers (FUIDR0/1).

The FUIDR is set (and write protected) by NXP prior to part shipment to provision a
pseudo-random software readable value, which can be (optionally) included as part of the
digital signature that is validated by the ISBC. This allows OEMs to create images that
can only pass secure boot on a specific chip. OEM can consider this to be an unalterable
highly unique value for the purposes of chip identification.

0 项奖励
回复