OTP on Layerscape

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OTP on Layerscape

2,888件の閲覧回数
mrmichaelt86
Contributor I

Hello.  Is there any sort of serial number or ID marked in the layerscape di?  Apart from Zone-of-Trust HSK, is there any ability to set an identifying serial number per device?  I would simply like to read a number in U-Boot and pass it to the Linux application, which is a unique number identifying the device.  If necessary, I will use the Security Secret Key, but exposing this in Linux Configuration space would be a security risk

0 件の賞賛
返信
4 返答(返信)

2,678件の閲覧回数
guignbt2v
Contributor III

Hi. Is there something similar for the LX2160?

0 件の賞賛
返信

2,881件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which exactly processor is in question?

0 件の賞賛
返信

2,864件の閲覧回数
mrmichaelt86
Contributor I

Processor in Question:  LS1046A

0 件の賞賛
返信

2,859件の閲覧回数
ufedor
NXP Employee
NXP Employee

Security fuse processor (SFP) contains 64-bit Factory Unique ID in two 32-bit registers (FUIDR0/1).

The FUIDR is set (and write protected) by NXP prior to part shipment to provision a
pseudo-random software readable value, which can be (optionally) included as part of the
digital signature that is validated by the ISBC. This allows OEMs to create images that
can only pass secure boot on a specific chip. OEM can consider this to be an unalterable
highly unique value for the purposes of chip identification.

0 件の賞賛
返信