OP-TEE U boot fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OP-TEE U boot fail

2,079件の閲覧回数
zcchai
Contributor I

Hello,

I have included OP TEE in ppa by enabling CONFIG_BUILD_OPTEE=y in file configs/build_lsdk.cfg, and build a composite firmware by running:

       $flex-builder -i mkfw -m ls1012afrwy -b qspi

and installed the firmware_ls1012afrwy_uboot_qspiboot.img by:

    =>load mmc 0:2 $load_addr irmware_ls1012afrwy_uboot_qspiboot.img 

     => sf probe 0:0;sf erase 0 +$filesize; sf write $load_addr  0 $filesize

     => sf erase 0x1d0000 +0x10000;

However, the board counld boot after that.

Reset Configuration Word (RCW):

       00000000: 0800000a 00000000 00000000 00000000

       00000010: 33050000 c000000c 40000000 00001800

       00000020: 00000000 00000000 00000000 000c47f2

       00000030: 00000000 1082a120 00000096 00000000

I2C:   ready

DRAM:  446 MiB

PPA Firmware: Version LSDK-18.09

SEC Firmware: 'loadables' present in config

loadables: 'trustedOS@1'

E/TC:0 Panic at core/arch/arm/mm/core_mmu.c:1745 <check_pa_matches_va>

E/TC:0 Call stack:

E/TC:0  0x000000009c00a8d0

Anyone know why it fails?

Thanks 

0 件の賞賛
返信
2 返答(返信)

1,830件の閲覧回数
bpe
NXP Employee
NXP Employee

Based on your later threads,  

you somehow have solved this problem. If it is  not correct, and the board that is experiencing difficulties is the

original NXP  LS1012FRWY, please open a Support Case for more help.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,830件の閲覧回数
zcchai
Contributor I

Hi Platon,

Thanks. Yes, I have solved the problem. The solution is described in my reply to this threads.

0 件の賞賛
返信