OOBE DEMO - SD CARD - LINUX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OOBE DEMO - SD CARD - LINUX

3,035件の閲覧回数
jeremykersale
Contributor I

Hello,

I would like to boot with a SDCARD the OOBE DEMO but i can't find the documentation for linux. If someone can give me a link about that it would be wonderful .

Ps: I have a TWR-LS1021A and i'm on Ubuntu.

Thank you !

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,768件の閲覧回数
jeremykersale
Contributor I

Hello again !

First, thank you for this help.

Now, I have a problem when i want to boot. Here is the script :

####START####

=>

U-Boot SPL 2014.01Layerscape-SDK-V1.1+g2b4d7d7 (Aug 29 2014 - 14:45:50)

U-Boot 2014.01Layerscape-SDK-V1.1+g2b4d7d7 (Aug 29 2014 - 14:45:50)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 20000000 00404000 60025a00 21042000

       00000020: 00000000 00000000 00000000 01038000

       00000030: 20024800 001b1200 00000000 00000000

Board: LS1021ATWR

I2C:   ready

DRAM:  1 GiB (DDR3, 32-bit, CL=10, ECC off)

MMC:   FSL_SDHC: 0

*** Warning - bad CRC, using default environment

In:    serial

Out:   serial

Err:   serial

SATA link 0 timeout.

AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode

flapio slum part ccc

scanning bus fo.

Found 0 device(s).

NeTSEC1 [PRIME], eTSEC2, eTSEC3

=>

=> setenv bootargs console=ttyS0,115200 ip=dhcp root=/dev/mmcblk0p1 rootwait

=> setenv load_kernel ext2load mmc :1 82000000 boot/uImage-3.12.0+

=> setenv load_dtb ext2load mmc :1 8f000000 boot/devicetree-uImage-ls1021a-twr.dtb

=> setenv bootcmd mmc rescan\; run load_kernel load_dtb\; bootm 82000000 - 8f000000

=> saveenv

Saving Environment to MMC...

Writing to MMC(0)... done

=> mmc rescan

=> ext2load mmc :1 82000000 boot/uImage-3.12.0+

3149256 bytes read in 295 ms (10.2 MiB/s)

=> mmc rescan

=> ext2load mmc :1 8f000000 boot/devicetree-uImage-ls1021a-twr.dtb

21717 bytes read in 143 ms (147.5 KiB/s)

=> bootm 82000000 - 8f000000

## Booting kernel from Legacy Image at 82000000 ...

   Image Name:   Linux-3.12.0+

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3149192 Bytes = 3 MiB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 8f000000

   Booting using the fdt blob at 0x8f000000

   Loading Kernel Image ... OK

   Loading Device Tree to bef0e000, end bef164d4 ... OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

#### END ####

There is nothing more after that.

I'm using a SDK V1.2 because the U-boot of the SDK V2.0 don't run.

By the way, i put on the SDCard :

- u-boot-with-spl-pbl-ls1021atwr_sdcard-2013.10+fslgit-r0.bin

then on mmcblk0p1 ( ext4 ), i put the fsl-image-full.

If someone have a idea it would be wonderful.

Thank you !!

0 件の賞賛
返信

2,768件の閲覧回数
bpe
NXP Employee
NXP Employee

SD card deployment instructions for your board can be found here:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-B47BE51A-7486-400A-9C3E-7...

General preparation steps are given here:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-E026CFFC-9C88-40CB-9C62-2...

Use fsl-image-full or fsl-image-core rootfs if you wish to have most packages pre-installed.

Pre-built images for your board can be found here:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

Browse the SDK documentation for a description of the functionality you are interested in:

https://freescale.sdlproducts.com/LiveContent/web/pub.xql?c=t&action=home&pub=QorIQ_SDK&lang=en-US


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------