OCRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OCRAM

1,072件の閲覧回数
VL38
Contributor I

Hello,

I'm wondering if it is possible to boot BL31 in OCRAM using LX2160A-RDB board. I'm doing nasty things obviously (not even ashamed !...). It's a 2MB memory, 256kB are used and BL31 is not oversized.

I tried to r/w in the free space but custom memcpy() function from driver is blocking at the very first byte to write.

Any clue ?

0 件の賞賛
返信
1 返信

1,021件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Hello, it isn't possible, BL31 uses DDR memory space, not OCRAM.

Please refer to the following in plat/nxp/common/include/default/plat_default_def.h.

#define BL31_BASE NXP_SECURE_DRAM_ADDR

 

BR.

0 件の賞賛
返信