NAND Access in u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND Access in u-boot

12,718 Views
jagadiswar_rao
Contributor I

Hi Team,

we are using ls2088a custom board, we are using  NAND and QSPI  are connected to IFC with different chip select .Can we able to access NAND in QSPI-Boot.

Labels (1)
0 Kudos
Reply
8 Replies

12,205 Views
ufedor
NXP Employee
NXP Employee

Please explain how QSPI is connected to IFC (attach corresponding schematics).

0 Kudos
Reply

12,201 Views
jagadiswar_rao
Contributor I

Hi Ufedor,

I have attached the schematic as pdf format of the QSPI connection to IFC.

0 Kudos
Reply

12,201 Views
ufedor
NXP Employee
NXP Employee

Picture quality is not suitable for inspection - please provide PDF.

0 Kudos
Reply

12,199 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> NAND and QSPI  are connected to IFC

In the provided schematics only NAND devices are connected to the IFC.

NAND has to be accessible after QSPI boot assuming that RCW with correct signals multiplexing is applied.

0 Kudos
Reply

12,201 Views
jagadiswar_rao
Contributor I

Hi

attached a schematic file check this one as a reference.How can we able to access nand on qspi-boot for this.

0 Kudos
Reply

12,201 Views
ufedor
NXP Employee
NXP Employee

There are no obvious errors in the QSPI_3.pdf.

> How can we able to access nand on qspi-boot for this.

Sorry, what do you mean?

0 Kudos
Reply

12,200 Views
jagadiswar_rao
Contributor I

required to load kernel on NAND flash from u-boot which is booted from qspi flash.Currently i am using LS2088ardb_qspi_defconfig for compilation of u-boot in this i am not able to access NAND in u-boot prompt.

attaching u-boot logs.

0 Kudos
Reply

12,200 Views
ufedor
NXP Employee
NXP Employee

There is no hardware issue with the design.

Please create separate question for the U-Boot "nand" issue.

0 Kudos
Reply