Multiple SATA devices using FIS on LS1021

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple SATA devices using FIS on LS1021

3,101 Views
otavioborges
Contributor III

I am currently designing a custom board that requires two SATA drives. Reading through LS1021 reference manual I noticed that the peripheral supports FIS multiplexing. But I am having a hard time finding a simple enough SATA controller. Any suggestions?

Would a simple lane multiplexer, with one selection GPIO work for this, like PI2DBS6212?

0 Kudos
Reply
5 Replies

3,080 Views
otavioborges
Contributor III

I'll probably change to the ls1024. Any concerns shifting the project from ls1021 to ls1024?

0 Kudos
Reply

3,075 Views
ufedor
NXP Employee
NXP Employee

It should be considered that NXP LSDK does not support LS1024A.

0 Kudos
Reply

3,091 Views
otavioborges
Contributor III

Does NXP provide any example or application note on this matter? Either for LS1021 or other layerscape core?

0 Kudos
Reply

3,085 Views
ufedor
NXP Employee
NXP Employee

There is no such application note.

0 Kudos
Reply

3,096 Views
ufedor
NXP Employee
NXP Employee

LS1021A SATA controller supports port multiplier operation. but there is no solution recommended by NXP either using a port multiplier chip or high-speed lane multiplexer.

 

0 Kudos
Reply