Multiple SATA devices using FIS on LS1021

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple SATA devices using FIS on LS1021

3,230件の閲覧回数
otavioborges
Contributor III

I am currently designing a custom board that requires two SATA drives. Reading through LS1021 reference manual I noticed that the peripheral supports FIS multiplexing. But I am having a hard time finding a simple enough SATA controller. Any suggestions?

Would a simple lane multiplexer, with one selection GPIO work for this, like PI2DBS6212?

0 件の賞賛
返信
5 返答(返信)

3,209件の閲覧回数
otavioborges
Contributor III

I'll probably change to the ls1024. Any concerns shifting the project from ls1021 to ls1024?

0 件の賞賛
返信

3,204件の閲覧回数
ufedor
NXP Employee
NXP Employee

It should be considered that NXP LSDK does not support LS1024A.

0 件の賞賛
返信

3,220件の閲覧回数
otavioborges
Contributor III

Does NXP provide any example or application note on this matter? Either for LS1021 or other layerscape core?

0 件の賞賛
返信

3,214件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no such application note.

0 件の賞賛
返信

3,225件の閲覧回数
ufedor
NXP Employee
NXP Employee

LS1021A SATA controller supports port multiplier operation. but there is no solution recommended by NXP either using a port multiplier chip or high-speed lane multiplexer.

 

0 件の賞賛
返信