Modify LS1046ardb.h file n uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Modify LS1046ardb.h file n uboot

1,153 Views
rashmikj
Contributor III

Hi,

We have custom board using LS1046a processor . The board is similar to LS1046ardb kit. I need to modify Ls1046ardb.h as per my board. I am unable to understand certain config options and address/values used in this file. Is there any documentation for the same.Kindly help.

Labels (1)
0 Kudos
Reply
1 Reply

1,116 Views
bpe
NXP Employee
NXP Employee

If you wish to identify the configuration macros you need to modify for your
home design board, the best approach is to go through the initialization code
of the original NXP design your own board  was  modeled after. For LS1046A-RDB,
this code is located here.

The code is reasonably compact and shows how various board-specific configuration
macros are used.

u-Boot global configuration options are documented in the main u-Boot readme file.

For the macros you cannot find in any of the above, search the source to see
where and how they are used or ask more specifically.

Macros that start with CONFIG_SYS_ are unlikely to need to be modified. If you
are to change any of them, make sure you understand fully what you are doing,
which basically means, again, look how the code uses them.

Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply