Management Signals for SERDES in LS1021A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Management Signals for SERDES in LS1021A

971件の閲覧回数
deepaknaiknavar
Contributor II

Hello,

Is it required to provide Management signals (MDC/MDIO) to the external PHY device for the SGMII interface in LS1021A? I mean does the Serdes interface itself can be used for the configuration PHY chip instead of the MDC/MDIO signals?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

841件の閲覧回数
bpe
NXP Employee
NXP Employee

SGMII specification provides only for transferring  link status updates
over the SGMII link. Refer to SGMII Spesc, Section "Control Information
Exchanged Between Links". There are no provisions for setting or reading
any PHY register over SGMII. Thus, if you wish to have full control
over your PHY, yes,  you need to connect it to an out-of-band management
interface.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

841件の閲覧回数
erdani80
Contributor III

Probably you could have a look at theTBI registers inside the eTSEC controller.

If you are planning to use a SFP you could also use fixed phy controllers in linux to get a connection.

0 件の賞賛
返信