MC version upgrade with DPDK application compatibility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC version upgrade with DPDK application compatibility

跳至解决方案
1,651 次查看
jackho
Contributor IV

Hi,

We are running DPDK version 19.11.6-rc1 with MC version 10.35, now we want to upgrade MC version to 10.36, some questions below want to confirm with you:

1. Does MC firmware version have a compatibility problem with DPDK version?

2. From the MC binary CHANGELOG.md file content, it seems MC 10.36 fix some dpaa2 issue.

Is it will affect DPDK initial flow? If yes, is there anything we should know to modify DPDK initial flow to fit MC version upgrade?

Thank you.

BR,

Jack Ho

0 项奖励
回复
1 解答
1,578 次查看
yipingwang
NXP TechSupport
NXP TechSupport

One more thing

Customer has not clarified if they are using the latest commits from NXP 19.11-qoriq branch

https://github.com/NXP/dpdk/

branch: 19.11-qroiq

 

They will need minimum  tag: LSDK20.04-isc-16

MC 10.36 compatibility was fixed at: https://github.com/NXP/dpdk/commit/ad8138fa3e85e557d4b6e29e72851b23f1a9cfd5

The latest tag is : LSDK20.04-isc-19

在原帖中查看解决方案

4 回复数
1,623 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Confirming with NXP DPDK team.

0 项奖励
回复
1,613 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I got confirmation from NXP DPDK development team.

MC binaries are typically backward compatible. So it will work without any issue with DPDK 19.11.6

I will also suggest, it will be better to migrate to MC 10.38.1

0 项奖励
回复
1,598 次查看
jackho
Contributor IV

Hi @yipingwang

Actually, we face an issue when upgrade MC version from 10.35 to 10.36, dpdk version is based on 19.11-rc6, we are using following method to create dpdk: 

echo dpni.2 > /sys/bus/fsl-mc/drivers/fsl_dpaa2_eth/unbind
restool dpni destroy dpni.2
export DPDMAI_COUNT=0
export DPIO_COUNT=16
/usr/local/dpdk/dpaa2/dynamic_dpl.sh dpni dpni -b 00:00:00:00:21:00
/usr/local/dpdk/dpaa2/dynamic_dpl.sh dpni.3 dpni -b 00:00:00:00:22:00
ls-addni --no-link --mac-addr=<mac address>
sleep 2
echo dprc.2 > /sys/bus/fsl-mc/drivers/vfio-fsl-mc/unbind

#DPD MUX is created as below with CUSTOM METHOD
restool dpdmux create --default-if=1 --num-ifs=2 --method DPDMUX_METHOD_CUSTOM --manip=DPDMUX_MANIP_NONE --option=DPDMUX_OPT_CLS_MASK_SUPPORT --container=dprc.1
restool dprc connect dprc.1 --endpoint1=dpdmux.0.0 --endpoint2=dpmac.3
restool dprc connect dprc.1 --endpoint1=dpdmux.0.1 --endpoint2=dpni.6
restool dprc connect dprc.1 --endpoint1=dpdmux.0.2 --endpoint2=dpni.2
restool dprc assign dprc.1 --object=dpdmux.0 --child=dprc.2 --plugged=1
echo dprc.2 > /sys/bus/fsl-mc/drivers/vfio-fsl-mc/bind

After dpdk init done, we start running our dpdk application,

it appears below error:

dpaa2_net: dpdmux_if_set_errors_behavior dpaa2_create_dpdmux_device err -22

dpaa2_net: Invalid dpdmux_id: 0

But in MC version 10.35 don't have these kinds of issue. we even try to upgrade MC version to 10.38, but issue still exist.

Could you help check with DPDK team what will cause this issue?

 Is it related to DPDK version?

Thanks

BR.

Jack Ho

0 项奖励
回复
1,579 次查看
yipingwang
NXP TechSupport
NXP TechSupport

One more thing

Customer has not clarified if they are using the latest commits from NXP 19.11-qoriq branch

https://github.com/NXP/dpdk/

branch: 19.11-qroiq

 

They will need minimum  tag: LSDK20.04-isc-16

MC 10.36 compatibility was fixed at: https://github.com/NXP/dpdk/commit/ad8138fa3e85e557d4b6e29e72851b23f1a9cfd5

The latest tag is : LSDK20.04-isc-19