Hi Team ,
Need help here.
We are trying change the MC version but it is not updating.
Can you please where I am doing wrong.
./flex-installer -b boot_LS_arm64_lts_5.10.tgz -r rootfs_lsdk2108_ubuntu_main_arm64.tgz -f firmware_ls2088ardb_norboot.img -d /dev/sdb
2) For MC version 30, below steps
tftp $load_addr mc_ls2088a_10.30.0.itb
erase 0x584A00000 0x584EFFFFF; cp.b 0xa0000000 0x584A00000 $filesize ;
qixis_reset altbank
=====
After above steps MC was not updated .
Next time by mistake I entered below command .
erase 0x580A00000 0x584EFFFFF
Now board not coming up as MC and other details erased.
Can you please help how to recover.
解決済! 解決策の投稿を見る。
ext2load mmc 0:2 0xa0000000 mc_ls2088a_10.32.0.itb
MMC: no card present
=> ext2load usb 0:2 0xa0000000 mc_ls2088a_10.32.0.itb
=> erase 0x584A00000 +$filesize
Bad address format
=> echo $filesize
Hi Can you please suggest which steps missing.
=> usb start
starting USB...
USB0: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
USB1: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus 0 for devices... 2 USB Device(s) found
scanning bus 1 for devices... 1 USB Device(s) found
scanning usb for storage devices... 1 Storage Device(s) found
=> ls usb 0:1
System Volume Information/
1211712 mc_ls2088a_10.32.0.itb
1 file(s), 1 dir(s)
=> ext2load usb 0:1 0xa0000000 mc_ls2088a_10.32.0.itb
** Unrecognized filesystem type **
I will Change from FAT32 to EXFAT will update
Please try to use command
fatload usb 0:1 0xa0000000 mc_ls2088a_10.32.0.itb
erase 0x580A00000 0x584EFFFFF : by mistake Given in 1st Board
erase 0x580000000 0x584EFFFFF : by mistake Given in 2nd Board
Can You Please how to recover My two LS2088 board. As now it stuck during Bootup time.
I assume that you can use SD u-boot on your target board.
Please deploy SD card on your host PC.
Please deploy bl2_sd.pbl to SD card with the following command.
sudo dd if=bl2_sd.pbl of=/dev/sdx bs=512 seek=8
Please deploy fip_uboot.bin to SD card with the following command.
sudo dd if=fip_uboot.bin of=/dev/sdx bs=512 seek=2048
Then configure the switch setting on your target board to boot from SD card.
Then recover NOR flash under SD u-boot prompt.
If you are using LS2088ARDB demo board, please use the following to deploy SD on the host.
$ wget https://www.nxp.com/lgfiles/sdk/lsdk2108/firmware_ls2088ardb_sdboot.img
$ flex-installer -f firmware_ls2088ardb_sdboot.img -d /dev/sdx
Please use the following command on bank0 to program bank4.
>> This Steps tried , It was not worked .
I will try ext2load in USB and update .
Thank you for your Quick Reply.
Please use the following command on bank0 to program bank4.
=> tftp 0xa0000000 mc_ls2088a_10.30.0.itb
=> erase 0x584A00000 +$filesize
=> cp.b 0xa0000000 0x584A00000 $filesize
If the networking cannot work, please copy mc_ls2088a_10.30.0.itb to USB or SD.
ext2load mmc 0:2 0xa0000000 mc_ls2088a_10.30.0.itb