M.2 SSD in LS1046 custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

M.2 SSD in LS1046 custom board

跳至解决方案
2,267 次查看
Ellu24
Contributor III

I am designing a hardware using LS1046. In our design, we are planning to use M.2 SSD PCIe3.0x4 instead of eMMC or SDcard. We are planning to connect M.2 SSD using USB -PCIe bridge. My questions are:

1) Can I use M.2 SSD instead of eMMC or SDcard and will the processor support the same?

2) Is it compatible for the processor to use the USB -PCIe bridge?

 

Thanking you in advance

 

标记 (1)
0 项奖励
回复
1 解答
2,232 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Ellu24,

LS1046A can boot from SD/eMMC. It cannot boot from SSD. So if you use SSD, you need to use some other boot source.

You are planning to use USB-PCIe bridge. I'm not sure why you do not plan to connect M.2 SSD directly to PCIe controller of LS1046A. This will give you very high throughput.

The USB controller of LS1046A complies with USB specification rev 3.0. You can plug-in anything that complies to the specification.

Regards,
Mrudang

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,233 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Ellu24,

LS1046A can boot from SD/eMMC. It cannot boot from SSD. So if you use SSD, you need to use some other boot source.

You are planning to use USB-PCIe bridge. I'm not sure why you do not plan to connect M.2 SSD directly to PCIe controller of LS1046A. This will give you very high throughput.

The USB controller of LS1046A complies with USB specification rev 3.0. You can plug-in anything that complies to the specification.

Regards,
Mrudang

0 项奖励
回复
2,222 次查看
Ellu24
Contributor III

Thank you very much for your reply.

0 项奖励
回复