LX2160a: Does U-Boot setup CCN508 and L3 cache?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LX2160a: Does U-Boot setup CCN508 and L3 cache?

2,112 次查看
bastian_schick
Contributor IV

Does U-Boot setup CCN508 and L3 cache?

I wonder because it does not seem that e.g. cluster 1 cores see RAM modifications of cluster 0 cores.

标记 (2)
0 项奖励
回复
1 回复

2,031 次查看
Pavel
NXP Employee
NXP Employee

There is single initialization code for CCN in -boot. See attachment. This file is available using the following path:

packages/firmware/u-boot/arch/arm/cpu/armv8/fsl-layerscape

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复