LX2160a: Does U-Boot setup CCN508 and L3 cache?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160a: Does U-Boot setup CCN508 and L3 cache?

2,120 Views
bastian_schick
Contributor IV

Does U-Boot setup CCN508 and L3 cache?

I wonder because it does not seem that e.g. cluster 1 cores see RAM modifications of cluster 0 cores.

Tags (2)
0 Kudos
Reply
1 Reply

2,039 Views
Pavel
NXP Employee
NXP Employee

There is single initialization code for CCN in -boot. See attachment. This file is available using the following path:

packages/firmware/u-boot/arch/arm/cpu/armv8/fsl-layerscape

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply