LX2160A - Synchronous Ethernet (SyncE) RCLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LX2160A - Synchronous Ethernet (SyncE) RCLK

31件の閲覧回数
fdekeers
Contributor I

Hi,

I'm using an LX2160A board.

From my understanding, the SerDes modules can use Synchronous Ethernet (SyncE) and recover the clock from the input SerDes signal. This clock is then available as RCLK0/1, with the related SerDes being selected with the register RECOV_CLK_SEL_RCLK0/1.

Can this recovered clock signal then be used to drive the SerDes modules, either the one that it was recovered from or another ?
Potentially as reference clock for the PLLS / PLLF ?

Thanks in advance.

タグ(1)
0 件の賞賛
返信
0 返答(返信)