LX2160A Memory Controller speed/clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LX2160A Memory Controller speed/clock

1,497件の閲覧回数
ash_law
Contributor III

Finally managed to get out LX2160ARDB up and running.

It shouldn't be that difficult, but that's a conversation for another day.

Question about memory controller frequency.

What is the max frequency? The system seems to say it's running at 700 MHz at boot. 

How does one go about changing the speed.

The reason I ask is that the first test we ran on it shows a processor that is severely memory access bound. (changing the CPU freq from 2 GHz to 1 GHz makes absolutely no difference to the processing time).

Thanks

0 件の賞賛
返信
1 返信

1,437件の閲覧回数
ufedor
NXP Employee
NXP Employee

Answers to your questions has to be based on the processor's Data Sheet and Reference Manual.

Current revisions of the LX2160A documents are confidential.

Please create a Technical Case and pose your questions in it:

https://nxpcommunity.force.com/community/CommunityContextPage?cf=General&subcf=Signpost+Section 

0 件の賞賛
返信