LSDK Code Aurora git clone extremely slow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LSDK Code Aurora git clone extremely slow

14,301 Views
dmitri_lechtchinski
Contributor III

Hello,

I'm currently trying to build firmware using LSDK flex-builder tool, and the git clone process is very slow, namely the https://source.codeaurora.org/external/qoriq/qoriq-components/linux.git repository. I getting a maximum of 80 KB/s download speed, and this it taking forever, additionally there is no way to "pause" a git clone process in case of network interruption.

Is there another mirror for this, or any alternative way to obtain the necessary sources?

Otherwise this process is not feasible for us.

Thanks,
Dmitri

8 Replies

13,931 Views
mcbridematt
Contributor III

There are at least two CodeAurora servers, it seems DNS anycast is used to choose which one you end up at.

siliconvalley.source.codeaurora.org is where I get sent (from Australia). It has been very slow the past week

https://portland.source.codeaurora.org/external/qoriq/ is much faster.

I believe there was an Asia (Singapore?) one but that must have disappeared when Qualcomm migrated away recently. As well as one for AWS us-east-1

Anyway, NXP should migrate or at least actively mirror to GitHub. I can't see CodeAurora lasting much longer now that the primary tenant (Qualcomm/QUIC) is/has moved out.

13,918 Views
dunk
Contributor III

Great thanks for this information.

0 Kudos
Reply

14,294 Views
ufedor
NXP Employee
NXP Employee

Which exactly command you have executed?

0 Kudos
Reply

14,054 Views
mpersano
Contributor I

I've been having the same issue in the last couple of days, I'm trying to build an image but bitbake gets stuck trying to clone a git repository from codeaurora. I get around 60kb/s. Already tried different VPNs.

The exact command that bitbake is running is:

 

git -c core.fsyncobjectfiles=0 clone --bare --mirror "https://source.codeaurora.org/external/imx/linux-imx.git"

 

0 Kudos
Reply

14,093 Views
dsouthwi
Contributor III

Same for me, this repository is nearly unusable.

 

$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux -b LSDK-21.08
Cloing https://source.codeaurora.org/external/qoriq/qoriq-components/linux release LSDK-21.08
Cloning into 'linux'...
remote: Enumerating objects: 10516405, done.
remote: Counting objects: 100% (28/28), done.
remote: Compressing objects: 100% (5/5), done.
Receiving objects:  12% (1313099/10516405), 635.59 MiB | 40.00 KiB/s

This will take days...

14,285 Views
dmitri_lechtchinski
Contributor III

I use LSDK 19.09, since the board we currently have is LX2160ARDB rev.1

The command is:

flex-builder -i mkfw -m lx2160ardb -b xspi

0 Kudos
Reply

14,271 Views
ufedor
NXP Employee
NXP Employee

I see about 9 MB/s in my case (Ubuntu on VirtualBox).

0 Kudos
Reply

13,936 Views
dunk
Contributor III

Hi ufedor,

Where do locate?

It's remarkably slow in Taiwan.

0 Kudos
Reply