LS2088A: MC error: Unsupported operation (status 0xb)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS2088A: MC error: Unsupported operation (status 0xb)

2,164 Views
QiujuYe
Contributor III

Hi,

Our board has one ls2088a chip, I build qspi image with LSDK1218,  after boot the board, when I use "ls-listni", then appear the error:

[root@TinyLSDK ~]$ ls-listni
MC error: Unsupported operation (status 0xb)
MC error: Unsupported operation (status 0xb)
dprc.1/dpni.3 (interface: eth0)
MC error: Unsupported operation (status 0xb)
MC error: Unsupported operation (status 0xb)
dprc.1/dpni.2 (interface: eth1)
MC error: Unsupported operation (status 0xb)
MC error: Unsupported operation (status 0xb)
dprc.1/dpni.1 (interface: eth2)
MC error: Unsupported operation (status 0xb)
MC error: Unsupported operation (status 0xb)
dprc.1/dpni.0 (interface: eth3)

 the ramdisk_rootfs_arm64.ext4.gz download from website automatically,

make: Entering directory '/home/qiuju/work/flexbuild_lsdk1812/packages/rfs'
make[1]: Entering directory '/home/qiuju/work/flexbuild_lsdk1812/packages/rfs'
--2020-09-17 08:17:54--  https://www.nxp.com/lgfiles/sdk/lsdk/ramdisk_rootfs_arm64.ext4.gz
Resolving www.nxp.com (www.nxp.com)... 104.111.211.197
Connecting to www.nxp.com (www.nxp.com)|104.111.211.197|:443... connected.
HTTP request sent, awaiting response... 200 OK
Length: 17603336 (17M) [application/x-gzip]
Saving to: 'ramdisk_rootfs_arm64.ext4.gz'
ramdisk_rootfs_arm64.ex 100%[===============================>]  16.79M  5.96MB/s    in 2.8s
2020-09-17 08:17:58 (5.96 MB/s) - 'ramdisk_rootfs_arm64.ext4.gz' saved [17603336/17603336]
 
the last boot log as followings, it shows NXP LSDK Tiny 19.06 , but I use lsdk1812 version, the mc version is "fsl-mc: Management Complex booted (version: 10.12.0, boot status: 0x1)", so whether the download ramdisk version is wrong ?
 
Starting syslogd/klogd: done
NXP LSDK Tiny 19.06 TinyLSDK ttyS0
TinyLSDK login: root
[root@TinyLSDK ~]$ cat /etc/version
20190610024753
[root@TinyLSDK ~]$ cat /etc/timestamp
20190610025624
[root@TinyLSDK ~]$ cat /etc/hostname
TinyLSDK
 
 
Best  Regards
Qiuju.ye
Labels (1)
0 Kudos
Reply
3 Replies

2,159 Views
Pavel
NXP Employee
NXP Employee

There is the following message dump on our LS2077ARDB board. See below.

Test your board using LSDK2004 or LSDK1909.

 

NXP LSDK tiny 1909 (based on Yocto)

TinyLinux login: root

root@TinyLinux:~# ls-listni

dprc.1/dpni.0 (interface: eth0, end point: dpmac.5)

root@TinyLinux:~#

 

Have a great day,
Pavel Chubakov

0 Kudos
Reply

2,156 Views
QiujuYe
Contributor III

Hi Pavel Chubakov,

Thanks for your help,  we could not change the lsdk version, our customers point the LSDK1218 version.

Can you give me a packet version ramdisk_rootfs_arm64.ext4.gz like as followings to try:

hwclock: can't open '/dev/misc/rtc': No such file or directory
Starting syslogd/klogd: done
QorIQ LSDK (NXP Reference Distro) 2.0 TinyDistro /dev/ttyS0
TinyDistro login: root
root@TinyDistro:/# cat /etc/version
20170712025733
root@TinyDistro:/#
root@TinyDistro:/# cat /etc/timestamp
20170712025957
root@TinyDistro:/# cat /etc/hostname
TinyDistro
 
Best Regards
Qiuju.ye
0 Kudos
Reply

2,117 Views
Pavel
NXP Employee
NXP Employee
0 Kudos
Reply