LS2088A: Disabling DP-DDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2088A: Disabling DP-DDR

2,272件の閲覧回数
ramasubramanian
Contributor I

Hello

We have custom hardware based on LS2088A.  We are not using AIOP interface.  Is that safe to disable DR-DDR?

Can we disable DP-DDR  and run MC on CPU DDR similar to that of LS2044A?

Regards

Rams

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,071件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Rams,

It is possible to disable DP-DDR and run MC on CPU DDR on LS2088A custom board. Some other customers also use this method in their products design. Please refer to the following to do modification in software.

1. Please disable “CONFIG_SYS_FSL_HAS_DP_DDR” in uboot to skip the DP DDR controller initialization.

I assume that you use the latest LSDK, in arch/arm/cpu/armv8/fsl-layerscape/Kconfig of u-boot source, please comment "select SYS_FSL_HAS_DP_DDR" for ARCH_LS2080A.

2. Every time ldpaa_dpni_setup called dpni_get_attributes, it will pass a value and tell mc to write all attributes to address 0x6100690000, and if dpddr is not on board or dpddr is not initialized appropriately, mc will hang after access this memory. Please do the following modification, just add one line to clear dflt_dpni memroy after allocated with malloc, as below…

 

    dflt_dpni = (struct fsl_dpni_obj *)malloc(sizeof(struct fsl_dpni_obj));

 

    if (!dflt_dpni) {

 

        printf("No memory: malloc() failed\n");

 

        err = -ENOMEM;

 

        goto err_malloc;

 

     _memset(dflt_dpni, 0, sizeof(struct fsl_dpni_obj));

... ...


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,071件の閲覧回数
ramasubramanian
Contributor I

Hi,

Thanks for the response.  We will test and come back if we have any issues.

Regards

Rams

0 件の賞賛
返信