Hi,
I'm trying to build U-Boot for LS1046ARDB on a Ubuntu 16.04 host using the flex-build framework.
The U-Boot fails with "Your GCC is older than 6.0 and is not supported". (My Version seems to be 5.04 ?)
How can I solve this issue?
Thanks
Philipp
Use Ubuntu 18.04 64bit version for SDK 18.06 building. There are no errors for this command if this Ubuntu is used.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------