LS2088 RDB LSDK does not boot from SD Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2088 RDB LSDK does not boot from SD Card

ソリューションへジャンプ
10,885件の閲覧回数
siyer
Contributor II

We have LS 2088 RDB boards Rev F. It boots fine from the NOR Flash but does not try to boot from the SD card (the SD card has LSDK - have tried with both online provided versions and locally built ones).

We have set the DIP Switches as follows

SW5- 11111111
SW3- 00010010
SW6- 11111111
SW4- 10111111
Sw9- 01000000
SW8- 01111111
SW7- 01000010

The board boots from NOR Flash even when the SD Card has been inserted.

 

Any suggestions for getting the board to boot from SD Card?

0 件の賞賛
返信
1 解決策
10,810件の閲覧回数
siyer
Contributor II

we found that the firmware of uboot on the board was 2016 version. We built and programmed the 2019 version in the NOR Flash. Now we can make it boot from SD Card. What is surprising is that these boards were bought 2 weeks back.. unclear why they are being shipped with old firmware.

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
10,811件の閲覧回数
siyer
Contributor II

we found that the firmware of uboot on the board was 2016 version. We built and programmed the 2019 version in the NOR Flash. Now we can make it boot from SD Card. What is surprising is that these boards were bought 2 weeks back.. unclear why they are being shipped with old firmware.

0 件の賞賛
返信
10,857件の閲覧回数
siyer
Contributor II

Also just want to indicate that after it boots up to the Linux distribution in NOR Flash, it can see all the partitions and files in the SD Card. So the card access and the LSDK on the card are good. It just does not use the SD card to boot. Is it the Uboot version? the version we have seems older than the ones in User guide

“U-Boot 2018.09-09790-gee0946537f (Nov 29 2018 - 21:21:15 +0800)”

0 件の賞賛
返信
10,866件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide U-Boot booting log for inspection.

0 件の賞賛
返信
10,849件の閲覧回数
siyer
Contributor II
 
0 件の賞賛
返信
10,846件の閲覧回数
siyer
Contributor II

the old file was incorrect. please use this..

0 件の賞賛
返信
10,845件の閲覧回数
siyer
Contributor II

“U-Boot 2016.092.0+ga06b209 (Mar 30 2017 – 01:15:01 +0000)”

oC: LS2088AE Rev1.1 (0x87090011)
Clock Configuration:
CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz
CPU3(A72):1800 MHz CPU4(A72):1800 MHz CPU5(A72):1800 MHz
CPU6(A72):1800 MHz CPU7(A72):1800 MHz
Bus: 700 MHz DDR: 1866.667 MT/s DP-DDR: 1600 MT/s
Reset Configuration Word (RCW):
00000000: 483038b8 48480048 00000000 00000000
00000010: 00000000 00000000 00a00000 00000000
00000020: 01001180 00002581 00000000 00000000
00000030: 00000c0b 00000000 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 00027000 00000000
00000070: 412a0000 00000000
Model: Freescale Layerscape 2080a RDB Board
Board: LS2088AE Rev1.1-RDB, Board Arch: V1, Board version: F, boot from vBank: 0
FPGA: v1.22
SERDES1 Reference : Clock1 = 156.25MHz Clock2 = 156.25MHz
SERDES2 Reference : Clock1 = 100MHz Clock2 = 100MHz
I2C: ready
DRAM: Initializing DDR....using SPD
Detected UDIMM 18ASF2G72AZ-2G6E2
Detected UDIMM 18ASF2G72AZ-2G6E2
DP-DDR: Detected UDIMM 18ASF2G72AZ-2G6E2
38.5 GiB
DDR 30.5 GiB (DDR4, 64-bit, CL=13, ECC on)
DDR Controller Interleaving Mode: 256B
DDR Chip-Select Interleaving Mode: CS0+CS1
DP-DDR 8 GiB (DDR4, 32-bit, CL=11, ECC on)
DDR Chip-Select Interleaving Mode: CS0+CS1
SEC0: RNG instantiated
SEC Firmware: config@1: no such config
SEC Firmware: error (-2)
SEC Firmware: Failed to load image
PSCI: PSCI does not exist.
Waking secondary cores to start from ffeff000
All (8) cores are up.
Using SERDES1 Protocol: 42 (0x2a)
Using SERDES2 Protocol: 65 (0x41)
Flash: 128 MiB
NAND: 2048 MiB
MMC: FSL_SDHC: 0
EEPROM: NXID v1
In: serial
Out: serial
Err: serial
Debug Server FW: Bad FIT image format
VID: Core voltage after adjustment is at 1023 mV
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
Found 0 device(s).
SCSI: Net: VID: Core voltage after adjustment is at 1054 mV
crc32+
fsl-mc: Booting Management Complex ... SUCCESS
fsl-mc: Management Complex booted (version: 10.1.6, boot status: 0x1)
PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 disabled
PCIe2: pcie@3600000 Root Complex: x1 gen1
PCIe3: pcie@3700000 Root Complex: no link
e1000: 68:05:ca:bd:3b:da
DPMAC1@xgmii [PRIME], DPMAC2@xgmii, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@xgmii, DPMAC6@xgmii, DPMAC7@xgmii, DPMAC8@xgmii, e1000#0
Warning: e1000#0 MAC addresses don't match:
Address in SROM is 68:05:ca:bd:3b:da
Address in environment is 68:05:ca:2b:9e:d3

Hit any key to stop autoboot: 0
fsl-mc: Deploying data path layout ... SUCCESS
## Loading kernel from FIT Image at a0000000 ...
Using 'config@1' configuration
Trying 'kernel@1' kernel subimage
Description: ARM64 Linux kernel
Created: 2017-03-29 17:54:55 UTC
Type: Kernel Image
Compression: gzip compressed
Data Start: 0xa00000d4
Data Size: 5483678 Bytes = 5.2 MiB
Architecture: AArch64
OS: Linux
Load Address: 0x80080000
Entry Point: 0x80080000
Verifying Hash Integrity ... OK
## Loading ramdisk from FIT Image at a0000000 ...
Using 'config@1' configuration
Trying 'ramdisk@1' ramdisk subimage
Description: Ramdisk
Created: 2017-03-29 17:54:55 UTC
Type: RAMDisk Image
Compression: uncompressed
Data Start: 0xa053eed4
Data Size: 37492773 Bytes = 35.8 MiB
Architecture: AArch64
OS: Linux
Load Address: unavailable
Entry Point: unavailable
Verifying Hash Integrity ... OK
## Loading fdt from FIT Image at a0000000 ...
Using 'config@1' configuration
Trying 'fdt@1' fdt subimage
Description: Flattened Device Tree blob
Created: 2017-03-29 17:54:55 UTC
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0xa053ae28
Data Size: 16425 Bytes = 16 KiB
Architecture: AArch64
Verifying Hash Integrity ... OK
Loading fdt from 0xa053ae28 to 0x90000000
Booting using the fdt blob at 0x90000000
Uncompressing Kernel Image ... OK
reserving fdt memory region: addr=80000000 size=10000
Loading Device Tree to 000000009fff8000, end 000000009ffff028 ... OK
WARNING: fdt_fixup_stdout: could not read serial1 alias: FDT_ERR_NOTFOUND

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Linux version 4.1.35-rt41 (jenkins@ceres) (gcc version 4.9.3 20150311 (prerelease) (Linaro GCC 4.9-2015.03) ) #1 SMP Thu Mar 30 01:18:48 CST 2017
[ 0.000000] CPU: AArch64 Processor [410fd082] revision 2
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] earlycon: Early serial console at MMIO 0x21c0600 (options '')
[ 0.000000] bootconsole [uart0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 16 MiB at 0x00000000fec00000
[ 0.000000] WARNING: x1-x3 nonzero in violation of boot protocol:
[ 0.000000] x1: 0000000000000000
[ 0.000000] x2: 0000000000000000
[ 0.000000] x3: 0000000080080000
[ 0.000000] This indicates a broken bootloader or old kernel
[ 0.000000] PERCPU: Embedded 18 pages/cpu @ffff80871ff31000 s34880 r8192 d30656 u73728
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 7870464
[ 0.000000] Kernel command line: console=ttyS1,115200 root=/dev/ram0 earlycon=uart8250,mmio,0x21c0600 ramdisk_size=0x2000000 default_hugepagesz=2m hugepagesz=2m hugepages=256
[ 0.000000] log_buf_len individual max cpu contribution: 4096 bytes
[ 0.000000] log_buf_len total cpu_extra contributions: 28672 bytes
[ 0.000000] log_buf_len min size: 16384 bytes
[ 0.000000] log_buf_len: 65536 bytes
[ 0.000000] early log buf free: 14524(88%)
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Dentry cache hash table entries: 4194304 (order: 13, 33554432 bytes)
[ 0.000000] Inode-cache hash table entries: 2097152 (order: 12, 16777216 bytes)
[ 0.000000] software IO TLB [mem 0xfac00000-0xfec00000] (64MB) mapped at [ffff80007ac00000-ffff80007ebfffff]
[ 0.000000] Memory: 31291612K/31981568K available (7770K kernel code, 582K rwdata, 3204K rodata, 480K init, 756K bss, 673572K reserved, 16384K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vmalloc : 0xffff000000000000 - 0xffff7bffbfff0000 (126974 GB)
[ 0.000000] vmemmap : 0xffff7bffc0000000 - 0xffff7fffc0000000 ( 4096 GB maximum)
[ 0.000000] 0xffff7bffc0000000 - 0xffff7c01dc800000 ( 8648 MB actual)
[ 0.000000] fixed : 0xffff7ffffabfd000 - 0xffff7ffffac00000 ( 12 KB)
[ 0.000000] PCI I/O : 0xffff7ffffae00000 - 0xffff7ffffbe00000 ( 16 MB)
[ 0.000000] modules : 0xffff7ffffc000000 - 0xffff800000000000 ( 64 MB)
[ 0.000000] memory : 0xffff800000000000 - 0xffff808720000000 (553472 MB)
[ 0.000000] .init : 0xffff800000b3a000 - 0xffff800000bb2000 ( 480 KB)
[ 0.000000] .text : 0xffff800000080000 - 0xffff800000b39934 ( 10983 KB)
[ 0.000000] .data : 0xffff800000bc4000 - 0xffff800000c55a00 ( 583 KB)
[ 0.000000] Hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=8.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=8
[ 0.000000] NR_IRQS:64 nr_irqs:64 0
[ 0.000000] ITS: /interrupt-controller@6000000/gic-its@6020000
[ 0.000000] ITS: allocated 8192 Devices @877d820000 (psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GIC: using LPI property table @0x000000877d830000
[ 0.000000] ITS: Allocated 1792 chunks for LPIs
[ 0.000000] CPU0: found redistributor 0 region 0:0x0000000006100000
[ 0.000000] CPU0: using LPI pending table @0x000000877d840000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] Architected cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000001] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
[ 0.008228] Console: colour dummy device 80x25
[ 0.012703] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=250000)
[ 0.023129] pid_max: default: 32768 minimum: 301
[ 0.027818] Security Framework initialized
[ 0.031962] Mount-cache hash table entries: 65536 (order: 7, 524288 bytes)
[ 0.038887] Mountpoint-cache hash table entries: 65536 (order: 7, 524288 bytes)
[ 0.046646] Initializing cgroup subsys memory
[ 0.051040] Initializing cgroup subsys hugetlb
[ 0.055593] hw perfevents: enabled with arm/armv8-pmuv3 PMU driver, 7 counters available
[ 0.063753] EFI services will not be available.
[ 0.068825] CPU1: Booted secondary processor
[ 0.068828] Detected PIPT I-cache on CPU1
[ 0.068833] CPU1: found redistributor 1 region 0:0x0000000006120000
[ 0.068849] CPU1: using LPI pending table @0x000000877da70000
[ 0.069016] CPU2: Booted secondary processor
[ 0.069019] Detected PIPT I-cache on CPU2
[ 0.069024] CPU2: found redistributor 100 region 0:0x0000000006140000
[ 0.069041] CPU2: using LPI pending table @0x000000877dab0000
[ 0.069214] CPU3: Booted secondary processor
[ 0.069216] Detected PIPT I-cache on CPU3
[ 0.069220] CPU3: found redistributor 101 region 0:0x0000000006160000
[ 0.069236] CPU3: using LPI pending table @0x000000877daf0000
[ 0.069406] CPU4: Booted secondary processor
[ 0.069409] Detected PIPT I-cache on CPU4
[ 0.069414] CPU4: found redistributor 200 region 0:0x0000000006180000
[ 0.069431] CPU4: using LPI pending table @0x000000877db20000
[ 0.069598] CPU5: Booted secondary processor
[ 0.069600] Detected PIPT I-cache on CPU5
[ 0.069604] CPU5: found redistributor 201 region 0:0x00000000061a0000
[ 0.069620] CPU5: using LPI pending table @0x000000877db60000
[ 0.069780] CPU6: Booted secondary processor
[ 0.069783] Detected PIPT I-cache on CPU6
[ 0.069789] CPU6: found redistributor 300 region 0:0x00000000061c0000
[ 0.069807] CPU6: using LPI pending table @0x000000877dba0000
[ 0.069977] CPU7: Booted secondary processor
[ 0.069979] Detected PIPT I-cache on CPU7
[ 0.069983] CPU7: found redistributor 301 region 0:0x00000000061e0000
[ 0.070000] CPU7: using LPI pending table @0x000000877dbe0000
[ 0.070036] Brought up 8 CPUs
[ 0.216945] SMP: Total of 8 processors activated.
[ 0.221682] CPU: All CPU(s) started at EL2
[ 0.225997] devtmpfs: initialized
[ 0.230831] DMI not present or invalid.
[ 0.234787] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.248965] pinctrl core: initialized pinctrl subsystem
[ 0.254665] NET: Registered protocol family 16
[ 0.289177] cpuidle: using governor ladder
[ 0.329160] cpuidle: using governor menu
[ 0.333132] fsl-mc bus type registered
[ 0.336916] MC object device driver fsl_mc_dprc registered
[ 0.342443] MC object device driver fsl_mc_allocator registered
[ 0.348463] vdso: 2 pages (1 code @ ffff800000bc9000, 1 data @ ffff800000bc8000)
[ 0.355924] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.363112] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.369316] Serial: AMBA PL011 UART driver
[ 0.374294] fsl_mc_bus 80c000000.fsl-mc: Root MC bus device probed
[ 0.390521] fsl_mc_bus 80c000000.fsl-mc: Freescale Management Complex Firmware version: 10.1.6
[ 1.291071] fsl-mc: Allocated dpmcp.19 to dprc.1 for atomic MC I/O
[ 1.331882] fsl_mc_dprc dprc.1: DPRC device bound to driver
[ 1.370033] arm-smmu 5000000.iommu: probing hardware configuration...
[ 1.376521] arm-smmu 5000000.iommu: SMMUv2 with:
[ 1.381173] arm-smmu 5000000.iommu: stage 1 translation
[ 1.386518] arm-smmu 5000000.iommu: stage 2 translation
[ 1.391866] arm-smmu 5000000.iommu: nested translation
[ 1.397124] arm-smmu 5000000.iommu: coherent table walk
[ 1.402475] arm-smmu 5000000.iommu: stream matching with 128 register groups, mask 0x7fff
[ 1.410801] arm-smmu 5000000.iommu: 64 context banks (0 stage-2 only)
[ 1.417375] arm-smmu 5000000.iommu: Supported page sizes: 0x60211000
[ 1.423861] arm-smmu 5000000.iommu: Stage-1: 48-bit VA -> 48-bit IPA
[ 1.430342] arm-smmu 5000000.iommu: Stage-2: 48-bit IPA -> 48-bit PA
[ 1.436830] arm-smmu 5000000.iommu: registered 1 master devices
[ 1.443233] vgaarb: loaded
[ 1.446064] SCSI subsystem initialized
[ 1.450020] usbcore: registered new interface driver usbfs
[ 1.455563] usbcore: registered new interface driver hub
[ 1.460942] usbcore: registered new device driver usb
[ 1.466204] i2c i2c-0: IMX I2C adapter registered
[ 1.470942] i2c i2c-0: can't use DMA
[ 1.474565] pps_core: LinuxPPS API ver. 1 registered
[ 1.479557] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 1.488763] PTP clock support registered
[ 1.492834] No BMan portals available!
[ 1.496729] QMan: Allocated lookup table at ffff000000b81000, entry count 65537
[ 1.504145] No QMan portals available!
[ 1.507987] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 1.514059] fsl-ifc 2240000.ifc: Freescale Integrated Flash Controller
[ 1.520642] fsl-ifc 2240000.ifc: IFC version 2.0, 8 banks
[ 1.526393] Switched to clocksource arch_sys_counter
[ 1.534112] NET: Registered protocol family 2
[ 1.538699] TCP established hash table entries: 262144 (order: 9, 2097152 bytes)
[ 1.546740] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes)
[ 1.553700] TCP: Hash tables configured (established 262144 bind 65536)
[ 1.560402] UDP hash table entries: 16384 (order: 7, 524288 bytes)
[ 1.566764] UDP-Lite hash table entries: 16384 (order: 7, 524288 bytes)
[ 1.573660] NET: Registered protocol family 1
[ 1.578171] RPC: Registered named UNIX socket transport module.
[ 1.584134] RPC: Registered udp transport module.
[ 1.588873] RPC: Registered tcp transport module.
[ 1.593604] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.600174] Trying to unpack rootfs image as initramfs...
[ 1.605747] rootfs image is not initramfs (no cpio magic); looks like an initrd
[ 1.641709] Freeing initrd memory: 36612K (ffff80002053f000 - ffff800022900000)
[ 1.649327] kvm [1]: interrupt-controller@c0e0000 IRQ5
[ 1.654581] kvm [1]: timer IRQ3
[ 1.657754] kvm [1]: Hyp mode initialized successfully
[ 1.664213] futex hash table entries: 2048 (order: 5, 131072 bytes)
[ 1.670576] audit: initializing netlink subsys (disabled)
[ 1.676021] audit: type=2000 audit(1.620:1): initialized
[ 1.684966] HugeTLB registered 2 MB page size, pre-allocated 256 pages
[ 1.691805] VFS: Disk quotas dquot_6.6.0
[ 1.695775] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 1.703044] NFS: Registering the id_resolver key type
[ 1.708141] Key type id_resolver registered
[ 1.712345] Key type id_legacy registered
[ 1.716463] fuse init (API version 7.23)
[ 1.720513] 9p: Installing v9fs 9p2000 file system support
[ 1.726554] io scheduler noop registered
[ 1.730520] io scheduler cfq registered (default)
[ 1.735332] Find msi-controller /interrupt-controller@6000000/gic-its@6020000
[ 1.743008] PCI host bridge /pcie@3600000 ranges:
[ 1.747755] IO 0x3000010000..0x300001ffff -> 0x00000000
[ 1.753277] MEM 0x3040000000..0x307fffffff -> 0x40000000
[ 1.758878] layerscape-pcie 3600000.pcie: PCI host bridge to bus 0000:00
[ 1.765627] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.771152] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 1.777377] pci_bus 0000:00: root bus resource [mem 0x3040000000-0x307fffffff] (bus address [0x40000000-0x7fffffff])
[ 1.788149] pci 0000:00:00.0: bridge configuration invalid ([bus 03-03]), reconfiguring
[ 1.816449] pci 0000:00:00.0: BAR 1: assigned [mem 0x3040000000-0x3043ffffff]
[ 1.823624] pci 0000:00:00.0: BAR 0: assigned [mem 0x3044000000-0x3044ffffff]
[ 1.830805] pci 0000:00:00.0: BAR 6: assigned [mem 0x3045000000-0x3045ffffff pref]
[ 1.838419] pci 0000:00:00.0: BAR 8: assigned [mem 0x3046000000-0x30460fffff]
[ 1.845592] pci 0000:00:00.0: BAR 7: assigned [io 0x1000-0x1fff]
[ 1.851720] pci 0000:01:00.0: BAR 1: assigned [mem 0x3046000000-0x304607ffff]
[ 1.858910] pci 0000:01:00.0: BAR 6: assigned [mem 0x3046080000-0x30460bffff pref]
[ 1.866522] pci 0000:01:00.0: BAR 0: assigned [mem 0x30460c0000-0x30460dffff]
[ 1.873709] pci 0000:01:00.0: BAR 3: assigned [mem 0x30460e0000-0x30460e3fff]
[ 1.880897] pci 0000:01:00.0: BAR 2: assigned [io 0x1000-0x101f]
[ 1.887039] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 1.892026] pci 0000:00:00.0: bridge window [io 0x1000-0x1fff]
[ 1.898153] pci 0000:00:00.0: bridge window [mem 0x3046000000-0x30460fffff]
[ 1.905439] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 1.912439] pci 0000:01:00.0: Signaling PME through PCIe PME interrupt
[ 1.919080] layerscape-pcie 3600000.pcie: failed to get PME IRQ: -6
[ 1.925377] layerscape-pcie 3600000.pcie: failed to initialize PME
[ 1.931629] PCI host bridge /pcie@3700000 ranges:
[ 1.936357] IO 0x3800010000..0x380001ffff -> 0x00000000
[ 1.941872] MEM 0x3840000000..0x387fffffff -> 0x40000000
[ 1.947452] layerscape-pcie 3700000.pcie: PCI host bridge to bus 0001:00
[ 1.954188] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 1.959703] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
[ 1.968714] pci_bus 0001:00: root bus resource [mem 0x3840000000-0x387fffffff] (bus address [0x40000000-0x7fffffff])
[ 1.979450] pci 0001:00:00.0: bridge configuration invalid ([bus 05-05]), reconfiguring
[ 1.987551] pci 0001:00:00.0: BAR 6: assigned [mem 0x3840000000-0x38400007ff pref]
[ 1.995159] pci 0001:00:00.0: PCI bridge to [bus 01]
[ 2.000211] pcieport 0001:00:00.0: Signaling PME through PCIe PME interrupt
[ 2.007280] layerscape-pcie 3700000.pcie: failed to get PME IRQ: -6
[ 2.013577] layerscape-pcie 3700000.pcie: failed to initialize PME
[ 2.019982] Freescale LS2 console driver
[ 2.023971] fsl-ls2-console: device fsl_mc_console registered
[ 2.029795] fsl-ls2-console: device fsl_aiop_console registered
[ 2.036908] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[ 2.043717] msm_serial: driver initialized
[ 2.047966] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 8, base_baud = 21875000) is a 16550A
[ 2.056869] console [ttyS1] disabled
[ 2.060470] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 8, base_baud = 21875000) is a 16550A
[ 2.069238] console [ttyS1] enabled
[ 2.069238] console [ttyS1] enabled
[ 2.076222] bootconsole [uart0] disabled
[ 2.076222] bootconsole [uart0] disabled
[ 2.084522] Unable to detect cache hierarcy from DT for CPU 0
[ 2.092619] brd: module loaded
[ 2.097350] loop: module loaded
[ 2.100826] ahci-qoriq 3200000.sata: controller can't do NCQ, turning off CAP_NCQ
[ 2.108324] ahci-qoriq 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 2.117282] ahci-qoriq 3200000.sata: flags: 64bit sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 2.126945] scsi host0: ahci-qoriq
[ 2.130432] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 196
[ 2.138487] ahci-qoriq 3210000.sata: controller can't do NCQ, turning off CAP_NCQ
[ 2.145977] ahci-qoriq 3210000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 2.154937] ahci-qoriq 3210000.sata: flags: 64bit sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 2.164542] scsi host1: ahci-qoriq
[ 2.168028] ata2: SATA max UDMA/133 mmio [mem 0x03210000-0x0321ffff] port 0x100 irq 197
[ 2.177737] of-flash 580000000.nor: do_map_probe() failed for type cfi_probe
[ 2.184838] of-flash 580000000.nor: do_map_probe() failed
[ 2.190659] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0x48
[ 2.197012] nand: Micron MT29F16G08ABACAWP
[ 2.201100] nand: 2048 MiB, SLC, erase size: 512 KiB, page size: 4096, OOB size: 224
[ 2.208845] nand: WARNING: 530000000.flash: the ECC used on your system is too weak compared to the one required by the NAND chip
[ 2.221519] Bad block table found at page 524160, version 0x01
[ 2.229281] Bad block table found at page 524032, version 0x01
[ 2.236068] nand_read_bbt: bad block at 0x000002d00000
[ 2.241202] nand_read_bbt: bad block at 0x000002d80000
[ 2.246784] fsl,ifc-nand 530000000.nand: IFC NAND device at 0x530000000, bank 2
[ 2.254462] m25p80 spi0.0: unrecognized JEDEC id bytes: c1, 7c, 07
[ 2.261091] libphy: Fixed MDIO Bus: probed
[ 2.265217] tun: Universal TUN/TAP device driver, 1.6
[ 2.270265] tun: (C) 1999-2004 Max Krasnyansky <[email protected]>
[ 2.276641] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.281653] mdio_bus 8b96000: Error while reading PHY16 reg at 2.2
[ 2.287883] mdio_bus 8b96000: Error while reading PHY16 reg at 3.3
[ 2.294108] mdio_bus 8b96000: Error while reading PHY17 reg at 2.2
[ 2.300334] mdio_bus 8b96000: Error while reading PHY17 reg at 3.3
[ 2.306561] mdio_bus 8b96000: Error while reading PHY18 reg at 2.2
[ 2.312784] mdio_bus 8b96000: Error while reading PHY18 reg at 3.3
[ 2.319010] mdio_bus 8b96000: Error while reading PHY19 reg at 2.2
[ 2.325232] mdio_bus 8b96000: Error while reading PHY19 reg at 3.3
[ 2.331450] libphy: Freescale XGMAC MDIO Bus: probed
[ 2.340902] Freescale FM module, FMD API version 21.1.0
[ 2.346160] Freescale FM Ports module
[ 2.349821] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 2.355418] fsl_dpa: FSL DPAA Ethernet driver
[ 2.359798] fsl_advanced: FSL DPAA Advanced drivers:
[ 2.364756] fsl_proxy: FSL DPAA Proxy initialization driver
[ 2.370352] fsl_dpa_shared: FSL DPAA Shared Ethernet driver
[ 2.375942] fsl_dpa_macless: FSL DPAA MACless Ethernet driver
[ 2.381709] fsl_oh: FSL FMan Offline Parsing port driver
[ 2.387047] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 2.394087] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 2.399857] e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k
[ 2.405681] e1000e: Copyright(c) 1999 - 2014 Intel Corporation.
[ 2.411911] e1000e 0000:01:00.0: Interrupt Throttling Rate (ints/sec) set to dynamic conservative mode
[ 2.496397] ata1: SATA link down (SStatus 0 SControl 300)
[ 2.516395] ata2: SATA link down (SStatus 0 SControl 300)
[ 2.543509] e1000e 0000:01:00.0 eth0: registered PHC clock
[ 2.548994] e1000e 0000:01:00.0 eth0: (PCI Express:2.5GT/s:Width x1) 68:05:ca:bd:3b:da
[ 2.556908] e1000e 0000:01:00.0 eth0: Intel(R) PRO/1000 Network Connection
[ 2.563786] e1000e 0000:01:00.0 eth0: MAC: 3, PHY: 8, PBA No: E46981-008
[ 2.570511] sky2: driver version 1.30
[ 2.574484] VFIO - User Level meta-driver version: 0.3
[ 2.582977] MC object device driver vfio-fsl-mc registered
[ 3.389023] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 3.395545] ehci-pci: EHCI PCI platform driver
[ 3.400003] ehci-platform: EHCI generic platform driver
[ 3.405256] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 3.411438] ohci-pci: OHCI PCI platform driver
[ 3.415891] ohci-platform: OHCI generic platform driver
[ 3.421209] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 3.426698] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 3.434522] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x00010010
[ 3.443239] xhci-hcd xhci-hcd.0.auto: irq 198, io mem 0x03100000
[ 3.449508] hub 1-0:1.0: USB hub found
[ 3.453258] hub 1-0:1.0: 1 port detected
[ 3.457303] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 3.462785] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 3.470464] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 3.478749] hub 2-0:1.0: USB hub found
[ 3.482498] hub 2-0:1.0: 1 port detected
[ 3.486533] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 3.492014] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[ 3.499864] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x00010010
[ 3.508576] xhci-hcd xhci-hcd.1.auto: irq 199, io mem 0x03110000
[ 3.514777] hub 3-0:1.0: USB hub found
[ 3.518535] hub 3-0:1.0: 1 port detected
[ 3.522541] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 3.528027] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[ 3.535700] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[ 3.543975] hub 4-0:1.0: USB hub found
[ 3.547731] hub 4-0:1.0: 1 port detected
[ 3.551795] usbcore: registered new interface driver usb-storage
[ 3.557938] mousedev: PS/2 mouse device common for all mice
[ 3.563708] i2c /dev entries driver
[ 3.567719] i2c i2c-0: Added multiplexed i2c bus 1
[ 3.579523] rtc-ds3232 2-0068: rtc core: registered ds3232 as rtc0
[ 3.585702] i2c i2c-0: Added multiplexed i2c bus 2
[ 3.590573] i2c i2c-0: Added multiplexed i2c bus 3
[ 3.595462] i2c i2c-0: Added multiplexed i2c bus 4
[ 3.600324] i2c i2c-0: Added multiplexed i2c bus 5
[ 3.605179] i2c i2c-0: Added multiplexed i2c bus 6
[ 3.610040] i2c i2c-0: Added multiplexed i2c bus 7
[ 3.614898] i2c i2c-0: Added multiplexed i2c bus 8
[ 3.619685] pca954x 0-0075: registered 8 multiplexed busses for I2C mux pca9547
[ 3.627181] 4-004c supply vcc not found, using dummy regulator
[ 3.635018] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 3.641644] CPUidle arm: CPU 0 failed to init idle CPU ops
[ 3.647164] sdhci: Secure Digital Host Controller Interface driver
[ 3.653336] sdhci: Copyright(c) Pierre Ossman
[ 3.657706] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.665472] sdhci-esdhc 2140000.esdhc: No vmmc regulator found
[ 3.671309] sdhci-esdhc 2140000.esdhc: No vqmmc regulator found
[ 3.716393] mmc0: SDHCI controller on 2140000.esdhc [2140000.esdhc] using ADMA 64-bit
[ 3.724521] MC object device driver fsl_dpaa2_caam registered
[ 3.730525] usbcore: registered new interface driver usbhid
[ 3.736089] usbhid: USB HID core driver
[ 3.743090] mc_restool driver registered
[ 3.751429] ce_paddr=0x818090000, ci_paddr=0x81c090000, portalid=9, prios=8
[ 3.758387] ce_size=0x1000, ci_size=0x1000
[ 3.763003] fsl_dpio_drv dpio.7: dpio: probed object 7
[ 3.768136] fsl_dpio_drv dpio.7: receives_notifications = 1
[ 3.773961] fsl_dpio_drv dpio.7: has_irq = 1
[ 3.783663] ce_paddr=0x818080000, ci_paddr=0x81c080000, portalid=8, prios=8
[ 3.790622] ce_size=0x1000, ci_size=0x1000
[ 3.795236] fsl_dpio_drv dpio.6: dpio: probed object 6
[ 3.800375] fsl_dpio_drv dpio.6: receives_notifications = 1
[ 3.806199] fsl_dpio_drv dpio.6: has_irq = 1
[ 3.815918] ce_paddr=0x818070000, ci_paddr=0x81c070000, portalid=7, prios=8
[ 3.822876] ce_size=0x1000, ci_size=0x1000
[ 3.827496] fsl_dpio_drv dpio.5: dpio: probed object 5
[ 3.832626] fsl_dpio_drv dpio.5: receives_notifications = 1
[ 3.838457] fsl_dpio_drv dpio.5: has_irq = 1
[ 3.848166] ce_paddr=0x818060000, ci_paddr=0x81c060000, portalid=6, prios=8
[ 3.855119] ce_size=0x1000, ci_size=0x1000
[ 3.859739] fsl_dpio_drv dpio.4: dpio: probed object 4
[ 3.864868] fsl_dpio_drv dpio.4: receives_notifications = 1
[ 3.870699] fsl_dpio_drv dpio.4: has_irq = 1
[ 3.880409] ce_paddr=0x818050000, ci_paddr=0x81c050000, portalid=5, prios=8
[ 3.887369] ce_size=0x1000, ci_size=0x1000
[ 3.891983] fsl_dpio_drv dpio.3: dpio: probed object 3
[ 3.897120] fsl_dpio_drv dpio.3: receives_notifications = 1
[ 3.902950] fsl_dpio_drv dpio.3: has_irq = 1
[ 3.912657] ce_paddr=0x818040000, ci_paddr=0x81c040000, portalid=4, prios=8
[ 3.919617] ce_size=0x1000, ci_size=0x1000
[ 3.924231] fsl_dpio_drv dpio.2: dpio: probed object 2
[ 3.929367] fsl_dpio_drv dpio.2: receives_notifications = 1
[ 3.935197] fsl_dpio_drv dpio.2: has_irq = 1
[ 3.944921] ce_paddr=0x818030000, ci_paddr=0x81c030000, portalid=3, prios=8
[ 3.951882] ce_size=0x1000, ci_size=0x1000
[ 3.956504] fsl_dpio_drv dpio.1: dpio: probed object 1
[ 3.961638] fsl_dpio_drv dpio.1: receives_notifications = 1
[ 3.967475] fsl_dpio_drv dpio.1: has_irq = 1
[ 3.977198] ce_paddr=0x818020000, ci_paddr=0x81c020000, portalid=2, prios=8
[ 3.984158] ce_size=0x1000, ci_size=0x1000
[ 3.988781] fsl_dpio_drv dpio.0: dpio: probed object 0
[ 3.993913] fsl_dpio_drv dpio.0: receives_notifications = 1
[ 3.999745] fsl_dpio_drv dpio.0: has_irq = 1
[ 4.005930] MC object device driver fsl_dpio_drv registered
[ 4.011633] No fsl,qman node
[ 4.014571] Freescale USDPAA process driver
[ 4.018753] fsl-usdpaa: no region found
[ 4.022584] Freescale USDPAA process IRQ driver
[ 4.029138] sdhci: Tuning procedure failed, falling back to fixed sampling clock
[ 4.036532] mmc0: tuning execution failed
[ 4.040535] mmc0: error -5 whilst initialising SD card
[ 4.040746] fsl_dpaa2_eth dpni.0: Insufficient queues. Steering is disabled
[ 4.051031] fsl_dpaa2_eth dpni.0: Probed interface ni0
[ 4.051049] MC object device driver fsl_dpaa2_eth registered
[ 4.055577] dpaa2_mac dpmac.8: Connected to xgmii PHY.
[ 4.059876] dpaa2_mac dpmac.7: Connected to xgmii PHY.
[ 4.064365] dpaa2_mac dpmac.6: Connected to xgmii PHY.
[ 4.068876] dpaa2_mac dpmac.5: Connected to xgmii PHY.
[ 4.073073] dpaa2_mac dpmac.4: Registered fixed PHY.
[ 4.077254] dpaa2_mac dpmac.3: Registered fixed PHY.
[ 4.081441] dpaa2_mac dpmac.2: Registered fixed PHY.
[ 4.085640] dpaa2_mac dpmac.1: Registered fixed PHY.
[ 4.085656] MC object device driver dpaa2_mac registered
[ 4.085678] MC object device driver dpaa2_ethsw registered
[ 4.085698] MC object device driver dpaa2_evb registered
[ 4.085718] MC object device driver fsl_dce_api registered
[ 4.088855] pps pps0: new PPS source ptp1
[ 4.088865] MC object device driver dpaa2_rtc registered
[ 4.088958] Initializing XFRM netlink socket
[ 4.109051] NET: Registered protocol family 10
[ 4.109348] sit: IPv6 over IPv4 tunneling driver
[ 4.109557] NET: Registered protocol family 17
[ 4.109566] NET: Registered protocol family 15
[ 4.109584] 8021q: 802.1Q VLAN Support v1.8
[ 4.109603] 9pnet: Installing 9P2000 support
[ 4.109629] Key type dns_resolver registered
[ 4.109877] registered taskstats version 1
[ 4.110097] fsl_generic: FSL DPAA Generic Ethernet driver
[ 4.114533] rtc-ds3232 2-0068: setting system clock to 2017-04-04 10:41:01 UTC (1491302461)
[ 4.187431] RAMDISK: gzip image found at block 0
[ 5.246568] VFS: Mounted root (ext2 filesystem) readonly on device 1:0.
[ 5.253211] devtmpfs: mounted
[ 5.256346] Freeing unused kernel memory: 480K (ffff800000b3a000 - ffff800000bb2000)
[ 5.264109] Freeing alternatives memory: 48K (ffff800000bb2000 - ffff800000bbe000)
INIT: version 2.88 booting
Starting udev
[ 5.368043] udevd[1049]: starting version 182
[ 5.588080] random: dd urandom read with 6 bits of entropy available
Populating dev cache
Running postinst /etc/rpm-postinsts/100-sysvinit-inittab...
Running postinst /etc/rpm-postinsts/101-inetutils-inetd...
Running postinst /etc/rpm-postinsts/102-inetutils-ftpd...
INIT: Entering runlevel: 5un-postinsts exists du
Configuring network interfaces... done.
Starting OpenBSD Secure Shell server: sshd
generating ssh RSA key...
generating ssh ECDSA key...
generating ssh DSA key...
generating ssh ED25519 key...
done.
Starting network benchmark server: netserver.
Starting system log daemon...0
Starting kernel log daemon...0
Starting internet superserver: xinetd.

QorIQ SDK (FSL Reference Distro) 2.0 ls2088ardb /dev/ttyS1

ls2088ardb login:

CTRL-A Z for help |115200 8N1 | NOR | Minicom 2.6.2 | VT102 | Offline

 

0 件の賞賛
返信
10,840件の閲覧回数
ufedor
NXP Employee
NXP Employee

You wrote:
> We have set the DIP Switches as follows
> SW3- 00010010
> SW4- 10111111
These settings are for NOR boot.

0 件の賞賛
返信
10,838件の閲覧回数
siyer
Contributor II

ok, what should it be for booting from SD Card? In the manual there are no other changes indicated to make it boot from SD card.

0 件の賞賛
返信
10,829件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS2085A/LS2088A Reference Design Board Getting Started Guide, Table 3. Switch configurations.

For SD boot:
SW3: 00100000
SW4[1]: 0

0 件の賞賛
返信
10,369件の閲覧回数
clopez
Contributor I

Is SD boot supported in LS2088ardb? This post makes it sound like it is, but the QorIQ LS2085A/LS2088A Reference Design Board Getting Started Guide, Table 3. Switch configurations footnote 1 for SD 2.0 says it is not.

0 件の賞賛
返信