LS2088 Kernel panic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2088 Kernel panic

1,580件の閲覧回数
ranga_yn
Contributor III

Hello NXP,

getting below kernel panic on bank 0 on Bank4 the board is booting fine with LSDK20.04 . what could be the possible error.

 

U-Boot 2018.03 (May 21 2020 - 00:19:35 +0530)

SoC: LS2088AE Rev1.1 (0x87090011)
Clock Configuration:
CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz
CPU3(A72):1800 MHz CPU4(A72):1800 MHz CPU5(A72):1800 MHz
CPU6(A72):1800 MHz CPU7(A72):1800 MHz
Bus: 700 MHz DDR: 1866.667 MT/s DP-DDR: 1600 MT/s
Reset Configuration Word (RCW):
00000000: 483038b8 48480048 00000000 00000000
00000010: 00000000 00000000 00a00000 00000000
00000020: 01001180 00002581 00000000 00000000
00000030: 00400c0b 00000000 00000000 00000000
00000040: 00000000 00000000 00000000 00000000
00000050: 00000000 00000000 00000000 00000000
00000060: 00000000 00000000 00027000 00000000
00000070: 412a0000 00040000
Model: Freescale Layerscape 2080a RDB Board
Board: LS2088AE Rev1.1-RDB, Board Arch: V1, Board version: F, boot from vBank: 0
FPGA: v1.22
SERDES1 Reference : Clock1 = 156.25MHz Clock2 = 156.25MHz
SERDES2 Reference : Clock1 = 100MHz Clock2 = 100MHz
I2C: ready
DRAM: Initializing DDR....using SPD
Detected UDIMM 18ADF2G72AZ-3G2E1
Detected UDIMM 18ADF2G72AZ-3G2E1
DP-DDR: Detected UDIMM 18ADF2G72AZ-3G2E1
39.9 GiB
DDR 31.9 GiB (DDR4, 64-bit, CL=13, ECC on)
DDR Controller Interleaving Mode: 256B
DDR Chip-Select Interleaving Mode: CS0+CS1
DP-DDR 8 GiB (DDR4, 32-bit, CL=11, ECC on)
DDR Chip-Select Interleaving Mode: CS0+CS1
SEC0: RNG instantiated
SEC Firmware: Bad firmware image (not a FIT image)
SEC0: RNG instantiated
Waking secondary cores to start from fbd22000
All (8) cores are up.
Using SERDES1 Protocol: 42 (0x2a)
Using SERDES2 Protocol: 65 (0x41)
Flash: 128 MiB
NAND: 2048 MiB
MMC: FSL_SDHC: 0
Loading Environment from Flash... OK
EEPROM: NXID v1
In: serial
Out: serial
Err: serial
VID: Core voltage after adjustment is at 1023 mV
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
Found 0 device(s).
SCSI: Net: PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 disabled
PCIe2: pcie@3600000 Root Complex: x1 gen1
PCIe3: pcie@3700000 Root Complex: no link
e1000: 68:05:ca:b1:44:cd
DPMAC1@xgmii [PRIME], DPMAC2@xgmii, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@xg mii, DPMAC6@xgmii, DPMAC7@xgmii, DPMAC8@xgmii, e1000#0
crc32+
fsl-mc: Booting Management Complex ... SUCCESS
fsl-mc: Management Complex booted (version: 10.20.4, boot status: 0x1)
Hit any key to stop autoboot: 0
starting USB...
USB0: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
USB1: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
scanning bus 1 for devices... 1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found

Device 0: device type unknown
... is now current device
** Bad device usb 0 **
** Bad device usb 0 **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
Scanning mmc 0:2...
Found U-Boot script /ls2088ardb_boot.scr
961 bytes read in 289 ms (2.9 KiB/s)
## Executing script at 80000000
25334272 bytes read in 1465 ms (16.5 MiB/s)
29725 bytes read in 193 ms (150.4 KiB/s)
## Flattened Device Tree blob at 90000000
Booting using the fdt blob at 0x90000000
Loading Device Tree to 000000009fff5000, end 000000009ffff41c ... OK
WARNING: SEC firmware not running, no kaslr-seed

Starting kernel ...

fsl-mc: Deploying data path layout ... SUCCESS
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd082]
[ 0.000000] Linux version 4.19.90-rt35-dirty (root@lab02-A01-39) (gcc version 7.5.0 (Ubuntu/Linaro 7.5.0-3ubuntu1~18.04)) #4 SMP PREEMPT RT Tue Sep 22 19:32: 21 IST 2020
[ 0.000000] Machine model: Freescale Layerscape 2088A RDB Board
[ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0600 (options '')
[ 0.000000] bootconsole [uart8250] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 32 MiB at 0x00000000f9c00000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x000000877fffffff ]
[ 0.000000] NUMA: NODE_DATA [mem 0x877ffcd440-0x877ffcec7f]
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] Normal [mem 0x0000000100000000-0x000000877fffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbdfffff]
[ 0.000000] node 0: [mem 0x0000008080000000-0x000000877fffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x000000877fffffff]
[ 0.000000] random: get_random_bytes called from start_kernel+0xa8/0x420 with crng_init=0
[ 0.000000] percpu: Embedded 25 pages/cpu s62144 r8192 d32064 u102400
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] ARM_SMCCC_ARCH_WORKAROUND_1 missing from firmware
[ 0.000000] CPU features: enabling workaround for EL2 vector hardening
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 7724544
[ 0.000000] Policy zone: Normal
[ 0.000000] Kernel command line: console=ttyS1,115200 earlycon=uart8250,mmio, 0x21c0600 root=PARTUUID=214159a0-04 rw rootwait default_hugepagesz=1024m hugepag esz=1024m hugepages=4 isolcpus=1-7
[ 0.000000] software IO TLB: mapped [mem 0xf5c00000-0xf9c00000] (64MB)
[ 0.000000] Memory: 26578072K/31389696K available (15100K kernel code, 1764K rwdata, 6268K rodata, 1536K init, 1008K bss, 4778856K reserved, 32768K cma-reser ved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=8, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=8.
[ 0.000000] rcu: RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000] No expedited grace period (rcu_normal_after_boot).
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=8
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000006100000
[ 0.000000] ITS [mem 0x06020000-0x0603ffff]
[ 0.000000] ITS@0x0000000006020000: allocated 8192 Devices @8761850000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000008761860000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x000000876187000 0
[ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000002] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 43980 46511100ns
[ 0.000151] Console: colour dummy device 80x25
[ 0.292894] Calibrating delay loop (skipped), value calculated using timer fr equency.. 50.00 BogoMIPS (lpj=100000)
[ 0.292897] pid_max: default: 32768 minimum: 301
[ 0.292928] Security Framework initialized
[ 0.309279] Dentry cache hash table entries: 4194304 (order: 14, 67108864 byt es)
[ 0.327660] Inode-cache hash table entries: 2097152 (order: 12, 16777216 byte s)
[ 0.327802] Mount-cache hash table entries: 65536 (order: 7, 524288 bytes)
[ 0.327928] Mountpoint-cache hash table entries: 65536 (order: 7, 524288 byte s)
[ 0.352207] ASID allocator initialised with 32768 entries
[ 0.420231] rcu: Hierarchical SRCU implementation.
[ 0.448280] Platform MSI: gic-its@6020000 domain created
[ 0.453678] PCI/MSI: /interrupt-controller@6000000/gic-its@6020000 domain cre ated
[ 0.461229] fsl-mc MSI: /interrupt-controller@6000000/gic-its@6020000 domain created
[ 0.469558] EFI services will not be available.
[ 0.480281] smp: Bringing up secondary CPUs ...
[ 0.540355] Detected PIPT I-cache on CPU1
[ 0.540369] GICv3: CPU1: found redistributor 1 region 0:0x0000000006120000
[ 0.540376] GICv3: CPU1: using allocated LPI pending table @0x000000876188000 0
[ 0.540393] CPU1: Booted secondary processor 0x0000000001 [0x410fd082]
[ 0.596403] Detected PIPT I-cache on CPU2
[ 0.596416] GICv3: CPU2: found redistributor 100 region 0:0x0000000006140000
[ 0.596422] GICv3: CPU2: using allocated LPI pending table @0x000000876189000 0
[ 0.596440] CPU2: Booted secondary processor 0x0000000100 [0x410fd082]
[ 0.652451] Detected PIPT I-cache on CPU3
[ 0.652460] GICv3: CPU3: found redistributor 101 region 0:0x0000000006160000
[ 0.652466] GICv3: CPU3: using allocated LPI pending table @0x00000087618a000 0
[ 0.652478] CPU3: Booted secondary processor 0x0000000101 [0x410fd082]
[ 0.708513] Detected PIPT I-cache on CPU4
[ 0.708527] GICv3: CPU4: found redistributor 200 region 0:0x0000000006180000
[ 0.708535] GICv3: CPU4: using allocated LPI pending table @0x00000087618b000 0
[ 0.708552] CPU4: Booted secondary processor 0x0000000200 [0x410fd082]
[ 0.764559] Detected PIPT I-cache on CPU5
[ 0.764568] GICv3: CPU5: found redistributor 201 region 0:0x00000000061a0000
[ 0.764575] GICv3: CPU5: using allocated LPI pending table @0x00000087618c000 0
[ 0.764587] CPU5: Booted secondary processor 0x0000000201 [0x410fd082]
[ 0.820622] Detected PIPT I-cache on CPU6
[ 0.820638] GICv3: CPU6: found redistributor 300 region 0:0x00000000061c0000
[ 0.820645] GICv3: CPU6: using allocated LPI pending table @0x00000087618d000 0
[ 0.820663] CPU6: Booted secondary processor 0x0000000300 [0x410fd082]
[ 0.876668] Detected PIPT I-cache on CPU7
[ 0.876679] GICv3: CPU7: found redistributor 301 region 0:0x00000000061e0000
[ 0.876685] GICv3: CPU7: using allocated LPI pending table @0x00000087618e000 0
[ 0.876697] CPU7: Booted secondary processor 0x0000000301 [0x410fd082]
[ 0.876741] smp: Brought up 1 node, 8 CPUs
[ 1.055241] SMP: Total of 8 processors activated.
[ 1.059967] CPU features: detected: GIC system register CPU interface
[ 1.066441] CPU features: detected: 32-bit EL0 Support
[ 1.072115] CPU: All CPU(s) started at EL2
[ 1.076241] alternatives: patching kernel code
[ 1.076842] devtmpfs: initialized
[ 1.089078] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ma x_idle_ns: 7645041785100000 ns
[ 1.098910] futex hash table entries: 2048 (order: 5, 131072 bytes)
[ 1.105604] xor: measuring software checksum speed
[ 1.148903] 8regs : 7674.000 MB/sec
[ 1.192925] 8regs_prefetch: 6688.000 MB/sec
[ 1.236925] 32regs : 8629.000 MB/sec
[ 1.280942] 32regs_prefetch: 7230.000 MB/sec
[ 1.285584] xor: using function: 32regs (8629.000 MB/sec)
[ 1.291017] pinctrl core: initialized pinctrl subsystem
[ 1.297674] DMI not present or invalid.
[ 1.302479] NET: Registered protocol family 16
[ 1.307385] audit: initializing netlink subsys (disabled)
[ 1.314285] cpuidle: using governor menu
[ 1.318564] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval___ _))
[ 1.325076] audit: type=2000 audit(1.308:1): state=initialized audit_enabled= 0 res=1
[ 1.334693] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 1.342469] DMA: preallocated 256 KiB pool for atomic allocations
[ 1.349637] Serial: AMBA PL011 UART driver
[ 1.355605] Machine: Freescale Layerscape 2088A RDB Board
[ 1.361497] SoC family: QorIQ LS2088A
[ 1.365177] SoC ID: svr:0x87090011, Revision: 1.1
[ 1.372523] fsl_mc_bus 80c000000.fsl-mc: MC firmware version: 10.20.4
[ 1.382057] fsl_mc_dprc dprc.1: DMA mask not set
[ 1.439559] HugeTLB registered 1.00 GiB page size, pre-allocated 4 pages
[ 1.525703] raid6: int64x1 gen() 1109 MB/s
[ 1.597718] raid6: int64x1 xor() 1000 MB/s
[ 1.669772] raid6: int64x2 gen() 1517 MB/s
[ 1.741821] raid6: int64x2 xor() 1473 MB/s
[ 1.813879] raid6: int64x4 gen() 2346 MB/s
[ 1.885930] raid6: int64x4 xor() 1642 MB/s
[ 1.957955] raid6: int64x8 gen() 1985 MB/s
[ 2.029992] raid6: int64x8 xor() 1609 MB/s
[ 2.102057] raid6: neonx1 gen() 2243 MB/s
[ 2.174090] raid6: neonx1 xor() 2496 MB/s
[ 2.246144] raid6: neonx2 gen() 2957 MB/s
[ 2.318172] raid6: neonx2 xor() 3146 MB/s
[ 2.390231] raid6: neonx4 gen() 3879 MB/s
[ 2.462277] raid6: neonx4 xor() 3463 MB/s
[ 2.534319] raid6: neonx8 gen() 4375 MB/s
[ 2.606366] raid6: neonx8 xor() 3671 MB/s
[ 2.610654] raid6: using algorithm neonx8 gen() 4375 MB/s
[ 2.616079] raid6: .... xor() 3671 MB/s, rmw enabled
[ 2.621067] raid6: using neon recovery algorithm
[ 2.626113] ACPI: Interpreter disabled.
[ 2.631163] vgaarb: loaded
[ 2.634124] SCSI subsystem initialized
[ 2.642605] usbcore: registered new interface driver usbfs
[ 2.648385] usbcore: registered new interface driver hub
[ 2.653800] usbcore: registered new device driver usb
[ 2.660080] i2c i2c-0: IMX I2C adapter registered
[ 2.665245] pps_core: LinuxPPS API ver. 1 registered
[ 2.670622] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giome tti <[email protected]>
[ 2.679843] PTP clock support registered
[ 2.683964] EDAC MC: Ver: 3.0.0
[ 2.687704] No BMan portals available!
[ 2.691751] QMan: Allocated lookup table at (____ptrval____), entry count 655 37
[ 2.699345] No QMan portals available!
[ 2.703305] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 2.709678] fsl-ifc 2240000.ifc: Freescale Integrated Flash Controller
[ 2.716297] fsl-ifc 2240000.ifc: IFC version 2.0, 8 banks
[ 2.722259] Advanced Linux Sound Architecture Driver Initialized.
[ 2.729107] clocksource: Switched to clocksource arch_sys_counter
[ 2.735336] VFS: Disk quotas dquot_6.6.0
[ 2.739382] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 2.746430] pnp: PnP ACPI: disabled
[ 2.756987] NET: Registered protocol family 2
[ 2.764445] tcp_listen_portaddr_hash hash table entries: 16384 (order: 8, 104 8576 bytes)
[ 2.773269] TCP established hash table entries: 262144 (order: 9, 2097152 byt es)
[ 2.781970] TCP bind hash table entries: 65536 (order: 9, 3670016 bytes)
[ 2.789714] TCP: Hash tables configured (established 262144 bind 65536)
[ 2.796941] UDP hash table entries: 16384 (order: 9, 2097152 bytes)
[ 2.804541] UDP-Lite hash table entries: 16384 (order: 9, 2097152 bytes)
[ 2.811819] NET: Registered protocol family 1
[ 2.828561] RPC: Registered named UNIX socket transport module.
[ 2.834510] RPC: Registered udp transport module.
[ 2.839236] RPC: Registered tcp transport module.
[ 2.843962] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 2.851118] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters av ailable
[ 2.859096] kvm [1]: 8-bit VMID
[ 2.862587] kvm [1]: vgic-v2@c0e0000
[ 2.866228] kvm [1]: GIC system register CPU interface enabled
[ 2.872206] kvm [1]: vgic interrupt IRQ1
[ 2.876234] kvm [1]: Hyp mode initialized successfully
[ 2.882983] Initialise system trusted keyrings
[ 2.888044] workingset: timestamp_bits=44 max_order=23 bucket_order=0
[ 2.902415] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 2.914716] NFS: Registering the id_resolver key type
[ 2.919805] Key type id_resolver registered
[ 2.924239] Key type id_legacy registered
[ 2.928273] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 2.935205] fuse init (API version 7.27)
[ 2.940012] 9p: Installing v9fs 9p2000 file system support
[ 2.947693] Key type asymmetric registered
[ 2.951810] Asymmetric key parser 'x509' registered
[ 2.956789] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 2 44)
[ 2.968323] io scheduler noop registered
[ 2.972269] io scheduler deadline registered
[ 2.976657] io scheduler cfq registered (default)
[ 2.981507] io scheduler mq-deadline registered
[ 2.986062] io scheduler kyber registered
[ 2.996973] layerscape-pcie 3600000.pcie: host bridge /soc/pcie@3600000 range s:
[ 3.006601] layerscape-pcie 3600000.pcie: IO 0x3000010000..0x300001ffff -> 0x00000000
[ 3.014750] layerscape-pcie 3600000.pcie: MEM 0x3040000000..0x307fffffff -> 0x40000000
[ 3.023124] layerscape-pcie 3600000.pcie: PCI host bridge to bus 0000:00
[ 3.029865] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 3.035936] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 3.042153] pci_bus 0000:00: root bus resource [mem 0x3040000000-0x307fffffff ] (bus address [0x40000000-0x7fffffff])
[ 3.065756] pci 0000:00:00.0: BAR 1: assigned [mem 0x3040000000-0x3043ffffff]
[ 3.072936] pci 0000:00:00.0: BAR 0: assigned [mem 0x3044000000-0x3044ffffff]
[ 3.080117] pci 0000:00:00.0: BAR 6: assigned [mem 0x3045000000-0x3045ffffff pref]
[ 3.087742] pci 0000:00:00.0: BAR 14: assigned [mem 0x3046000000-0x30460fffff ]
[ 3.095007] pci 0000:00:00.0: BAR 13: assigned [io 0x1000-0x1fff]
[ 3.101227] pci 0000:01:00.0: BAR 1: assigned [mem 0x3046000000-0x304607ffff]
[ 3.108422] pci 0000:01:00.0: BAR 6: assigned [mem 0x3046080000-0x30460bffff pref]
[ 3.116035] pci 0000:01:00.0: BAR 0: assigned [mem 0x30460c0000-0x30460dffff]
[ 3.123227] pci 0000:01:00.0: BAR 3: assigned [mem 0x30460e0000-0x30460e3fff]
[ 3.130419] pci 0000:01:00.0: BAR 2: assigned [io 0x1000-0x101f]
[ 3.136562] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 3.141813] pci 0000:00:00.0: bridge window [io 0x1000-0x1fff]
[ 3.147943] pci 0000:00:00.0: bridge window [mem 0x3046000000-0x30460fffff]
[ 3.155272] layerscape-pcie 3700000.pcie: host bridge /soc/pcie@3700000 range s:
[ 3.162631] layerscape-pcie 3700000.pcie: IO 0x3800010000..0x380001ffff -> 0x00000000
[ 3.170788] layerscape-pcie 3700000.pcie: MEM 0x3840000000..0x387fffffff -> 0x40000000
[ 3.179048] layerscape-pcie 3700000.pcie: PCI host bridge to bus 0001:00
[ 3.185790] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 3.191330] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus add ress [0x0000-0xffff])
[ 3.200355] pci_bus 0001:00: root bus resource [mem 0x3840000000-0x387fffffff ] (bus address [0x40000000-0x7fffffff])
[ 3.212423] pci 0001:00:00.0: BAR 6: assigned [mem 0x3840000000-0x38400007ff pref]
[ 3.220034] pci 0001:00:00.0: PCI bridge to [bus 01-ff]
[ 3.226999] EIN.iommu: stage 1 translation
[ 3.348002] arm-smmu 5000000.iommu: stage 2 translation
[ 3.353307] arm-smmu 5000000.iommu: nested translation
[ 3.358526] arm-smmu 5000000.iommu: coherent table walk
[ 3.363832] arm-smmu 5000000.iommu: stream matching with 128 register groups
[ 3.370963] arm-smmu 5000000.iommu: 64 context banks (0 stage-2 only)
[ 3.377487] arm-smmu 5000000.iommu: Supported page sizes: 0x61311000
[ 3.383922] arm-smmu 5000000.iommu: Stage-1: 48-bit VA -> 48-bit IPA
[ 3.390356] arm-smmu 5000000.iommu: Stage-2: 48-bit IPA -> 48-bit PA
[ 3.405734] brd: module loaded
[ 3.415024] loop: module loaded
[ 3.421412] ahci-qoriq 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0 x1 impl platform mode
[ 3.431000] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fb s pio slum part ccc sds apst
[ 3.445451] scsi host0: ahci-qoriq
[ 3.449069] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x1 00 irq 96
[ 3.457332] ahci-qoriq 3210000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0 x1 impl platform mode
[ 3.466382] ahci-qoriq 3210000.sata: flags: 64bit ncq sntf pm clo only pmp fb s pio slum part ccc sds apst
[ 3.480732] scsi host1: ahci-qoriq
[ 3.484287] ata2: SATA max UDMA/133 mmio [mem 0x03210000-0x0321ffff] port 0x1 00 irq 97
[ 3.492742] 580000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufac turer ID 0x000001 Chip ID 0x002801
[ 3.503093] Amd/Fujitsu Extended Query Table at 0x0040
[ 3.508234] Amd/Fujitsu Extended Query version 1.5.
[ 3.513297] number of CFI chips: 1
[ 3.518276] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0x48
[ 3.524624] nand: Micronthernet driver
[ 3.664619] fsl_advanced: FSL DPAA Advanced drivers:
[ 3.669577] fsl_proxy: FSL DPAA Proxy initialization driver
[ 3.675223] fsl_oh: FSL FMan Offline Parsing port driver
[ 3.681297] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 3.688556] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 3.694353] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 3.700182] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 3.706166] iommu: Adding device 0000:01:00.0 to group 0
[ 3.711885] e1000e 0000:01:00.0: Interrupt Throttling Rate (ints/sec) set to dynamic conservative mode
[ 3.777618] e1000e 0000:01:00.0 0000:01:00.0 (uninitialized): registered PHC clock
[ 3.781120] ata1: SATA link down (SStatus 0 SControl 300)
[ 3.809332] ata2: SATA link down (SStatus 0 SControl 300)
[ 3.856297] e1000e 0000:01:00.0 eth0: (PCI Express:2.5GT/s:Width x1) 68:05:ca :b1:44:cd
[ 3.864210] e1000e 0000:01:00.0 eth0: Intel(R) PRO/1000 Network Connection
[ 3.871091] e1000e 0000:01:00.0 eth0: MAC: 3, PHY: 8, PBA No: E46981-008
[ 3.877887] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.4.0-k
[ 3.884842] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 3.890468] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 3.898293] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 3.904555] sky2: driver version 1.30
[ 3.908829] usbcore: registered new interface driver r8152
[ 3.914477] usbcore: registered new interface driver asix
[ 3.919916] usbcore: registered new interface driver ax88179_178a
[ 3.926691] VFIO - User Level meta-driver version: 0.3
[ 3.932540] dwc3 3100000.usb3: Failed to get clk 'ref': -2
[ 3.938693] dwc3 3110000.usb3: Failed to get clk 'ref': -2
[ 3.945688] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 3.952428] ehci-pci: EHCI PCI platform driver
[ 3.956913] ehci-platform: EHCI generic platform driver
[ 3.962230] ehci-orion: EHCI orion driver
[ 3.966313] ehci-exynos: EHCI EXYNOS driver
[ 3.970561] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 3.976745] ohci-pci: OHCI PCI platform driver
[ 3.981234] ohci-platform: OHCI generic platform driver
[ 3.986538] ohci-exynos: OHCI EXYNOS driver
[ 3.990993] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 3.996481] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus nu mber 1
[ 4.004356] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000000002010010
[ 4.013821] xhci-hcd xhci-hcd.0.auto: irq 98, io mem 0x03100000
[ 4.020375] hub 1-0:1.0: USB hub found
[ 4.024130] hub 1-0:1.0: 1 port detected
[ 4.028305] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 4.033788] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus nu mber 2
[ 4.041443] xhci[ 4.177415] rtc-ds3232 2-0068: rtc core: registered ds3232 as rtc0
[ 4.183734] i2c i2c-0: Added multiplexed i2c bus 2
[ 4.188800] i2c i2c-0: Added multiplexed i2c bus 3
[ 4.193925] i2c i2c-0: Added multiplexed i2c bus 4
[ 4.198959] i2c i2c-0: Added multiplexed i2c bus 5
[ 4.203921] i2c i2c-0: Added multiplexed i2c bus 6
[ 4.208962] i2c i2c-0: Added multiplexed i2c bus 7
[ 4.213923] i2c i2c-0: Added multiplexed i2c bus 8
[ 4.218708] pca954x 0-0075: registered 8 multiplexed busses for I2C mux pca95 47
[ 4.228341] sp805-wdt c000000.wdt: registration successful
[ 4.234462] sp805-wdt c010000.wdt: registration successful
[ 4.240108] sp805-wdt c100000.wdt: registration successful
[ 4.245907] sp805-wdt c110000.wdt: registration successful
[ 4.251610] sp805-wdt c200000.wdt: registration successful
[ 4.257341] sp805-wdt c210000.wdt: registration successful
[ 4.263095] sp805-wdt c300000.wdt: registration successful
[ 4.268821] sp805-wdt c310000.wdt: registration successful
[ 4.276338] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 4.283348] CPUidle arm: CPU 0 failed to init idle CPU ops
[ 4.289175] sdhci: Secure Digital Host Controller Interface driver
[ 4.295349] sdhci: Copyright(c) Pierre Ossman
[ 4.300010] Synopsys Designware Multimedia Card Interface Driver
[ 4.306755] sdhci-pltfm: SDHCI platform and OF driver helper
[ 4.337124] mmc0: SDHCI controller on 2140000.esdhc [2140000.esdhc] using ADM A 64-bit
[ 4.348735] caam 8000000.crypto: device ID = 0x0a10040100000000 (Era
[ 4.355364] caam 8000000.val____))
[ 4.434850] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.19.90-rt35-dirty #4
[ 4.434851] Hardware name: Freescale Layerscape 2088A RDB Board (DT)
[ 4.434853] pstate: 00000005 (nzcv daif -PAN -UAO)
[ 4.434854] pc : (null)
[ 4.434854] lr : (null)
[ 4.434855] sp : 0000000000000000
[ 4.434856] x29: 0000000000000000 x28: 0000000000000000
[ 4.434859] x27: 0000000000000000 x26: 0000000000000000
[ 4.434861] x25: 0000000000000000 x24: 0000000000000000
[ 4.434863] x23: 0000000000000000 x22: 0000000000000000
[ 4.434864] x21: 0000000000000000 x20: 0000000000000000
[ 4.434866] x19: 0000000000000000 x18: 0000000000000000
[ 4.434868] x17: 0000000000000000 x16: 0000000000000000
[ 4.434870] x15: 0000000000000000 x14: 0000000000000000
[ 4.434871] x13: 0000000000000000 x12: 0000000000000000
[ 4.434873] x11: 0000000000000000 x10: 0000000000000000
[ 4.434875] x9 : 0000000000000000 x8 : 0000000000000000
[ 4.434877] x7 : 0000000000000000 x6 : 0000000000000000
[ 4.434878] x5 : 0000000000000000 x4 : 0000000000000000
[ 4.434880] x3 : 0000000000000000 x2 : 0000000000000000
[ 4.434882] x1 : 0000000000000000 x0 : 0000000000000000
[ 4.434884] Call trace:
[ 4.434885] (null)
[ 4.434889] Code: bad PC value
[ 4.566995] ---[ end trace 0000000000000001 ]---
[ 4.567245] Kernel panic - not syncing: Attempted to kill init! exitcode=0x00

0 件の賞賛
返信
0 返答(返信)