LS2085A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2085A

2,322件の閲覧回数
lucamoroni
Contributor I

As indicated on your Reference Design Board  to supply the  LS2085A device we used  the Multiphase Power controller IR3565A.  Now we have to program the multi-phase IR3565B. This component needs via I2C programming using a programming tool and a software called "IR DIGITAL POWER DESIGN CENTER (DPDC) GUI".  Device configuration and fault parameters are easily defined using the IR Digital Power Design Center (DPDC) GUI and stored in on-chip MTP.  But  the GUI  for Multi-Phase Devices, due to their proprietary technology, are generally restricted and require authorization. Without a license we can not program the  IR3565B device and then feed the LS2085A core. How can I get the licenses PowIrCenter? someone can give them to me?

ラベル(1)
0 件の賞賛
返信
1 返信

1,986件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP Semiconductors does not own the International Rectifier IR3565B Datasheet and IR GUI.

Look at the following document:

http://www.infineon.com/dgdl/an-0035.pdf?fileId=5546d462533600a40153559088d40f2d


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信