LS1088ARDB - reduced bandwidth connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1088ARDB - reduced bandwidth connection

19,649件の閲覧回数
reza_m
Contributor II

I have been running OpenWRT on the LS1088ARDB. I first tested a 1Gbps internet service plan to make sure the ports were working as specification and it worked using a v17.01.7 build. I then upgraded to v19.03 to get mwan3 support and now the maximum bandwidth i can get is about 70-100 Mbps. I have tried going back to the original image but my bandwidth still seems to be capped. What could the issue be? 

ラベル(1)
0 件の賞賛
返信
26 返答(返信)

2,455件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the image built from the latest OpenWrt release(on September 25th).

https://drive.google.com/file/d/1LlTlz8yzqdStnxW3U1mWl47IZHg86NDI/view?usp=sharing

0 件の賞賛
返信

2,468件の閲覧回数
reza_m
Contributor II

My issue still persists, what else can I try to solve it?

0 件の賞賛
返信

2,415件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please try the latest OpenWrt release, I uploaded it in the following link.

https://drive.google.com/file/d/1uxTNZzrc6Fu-wjaEL5arYe_QjSRnOp-Q/view?usp=sharing

 

NXP will release a new version OpenWrt on September 25th.

0 件の賞賛
返信

2,296件の閲覧回数
reza_m
Contributor II

I have tried building an image with the builder you have sent and I have tried the updated OpenWRT repo. Neither solution is working, what else can I try? Is there a hard reset I could trigger to wipe the flash drives?

0 件の賞賛
返信

2,472件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please use NXP latest released OpenWrt OpenWrt-19.04 

$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/openwrt

$ git checkout OpenWrt-19.04

In addition, please disable CONFIG_NETFILTER and CONFIG_CPU_FREQ in Linux kernel.

0 件の賞賛
返信

2,390件の閲覧回数
reza_m
Contributor II

I tried using the configuration settings and the build you suggested and my issue persists. 

0 件の賞賛
返信