LS1088ARDB - reduced bandwidth connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1088ARDB - reduced bandwidth connection

19,826 Views
reza_m
Contributor II

I have been running OpenWRT on the LS1088ARDB. I first tested a 1Gbps internet service plan to make sure the ports were working as specification and it worked using a v17.01.7 build. I then upgraded to v19.03 to get mwan3 support and now the maximum bandwidth i can get is about 70-100 Mbps. I have tried going back to the original image but my bandwidth still seems to be capped. What could the issue be? 

Labels (1)
0 Kudos
Reply
26 Replies

2,459 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the image built from the latest OpenWrt release(on September 25th).

https://drive.google.com/file/d/1LlTlz8yzqdStnxW3U1mWl47IZHg86NDI/view?usp=sharing

0 Kudos
Reply

2,472 Views
reza_m
Contributor II

My issue still persists, what else can I try to solve it?

0 Kudos
Reply

2,419 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please try the latest OpenWrt release, I uploaded it in the following link.

https://drive.google.com/file/d/1uxTNZzrc6Fu-wjaEL5arYe_QjSRnOp-Q/view?usp=sharing

 

NXP will release a new version OpenWrt on September 25th.

0 Kudos
Reply

2,300 Views
reza_m
Contributor II

I have tried building an image with the builder you have sent and I have tried the updated OpenWRT repo. Neither solution is working, what else can I try? Is there a hard reset I could trigger to wipe the flash drives?

0 Kudos
Reply

2,476 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please use NXP latest released OpenWrt OpenWrt-19.04 

$ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/openwrt

$ git checkout OpenWrt-19.04

In addition, please disable CONFIG_NETFILTER and CONFIG_CPU_FREQ in Linux kernel.

0 Kudos
Reply

2,394 Views
reza_m
Contributor II

I tried using the configuration settings and the build you suggested and my issue persists. 

0 Kudos
Reply