LS1088A Pin Configuration for eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1088A Pin Configuration for eMMC

Jump to solution
1,792 Views
zeroqruel
Contributor III

Hello,

I want to run 8 bus witdh eMMC on custom LS1088 based board. I have successfully activated emmc, but it is inited as 4 bus width every time. According to what I see in the datasheet and reference design, I need to configure the pins that are SPI by default in the OVDD section as SDHC_DAT4-7 in the HS Mux. I tried to do this on the DTS side but I am getting a syntax error.

&esdhc {
	status = "okay";
	compatible = "fsl,ls1088a-esdhc", "fsl,esdhc";
	non-removable;
	bus-width = <8>;
	clock-frequency = <200000000>;
	pinctrl-names = "default";
	pinctrl-0 = <&esdhc_pins>;
};

&fsl_lsiodev {
	esdhc_pins: esdhc-pins {
		fsl,pins = <
			LS1088A_SIGNAL(PAD_P3, SDHC_CLK, 0x06000049) /* SDHC_CLK */
			LS1088A_SIGNAL(PAD_P2, SDHC_CMD, 0x06000049) /* SDHC_CMD */
			LS1088A_SIGNAL(PAD_P1, SDHC_DATA0, 0x06000049) /* SDHC_DATA0 */
			LS1088A_SIGNAL(PAD_R2, SDHC_DATA1, 0x06000049) /* SDHC_DATA1 */
			LS1088A_SIGNAL(PAD_R1, SDHC_DATA2, 0x06000049) /* SDHC_DATA2 */
			LS1088A_SIGNAL(PAD_T1, SDHC_DATA3, 0x06000049) /* SDHC_DATA3 */
			LS1088A_SIGNAL(PAD_U1, SDHC_DATA4, 0x06000049) /* SDHC_DATA4 */
			LS1088A_SIGNAL(PAD_R3, SDHC_DATA5, 0x06000049) /* SDHC_DATA5 */
			LS1088A_SIGNAL(PAD_T3, SDHC_DATA6, 0x06000049) /* SDHC_DATA6 */

			LS1088A_SIGNAL(PAD_V1, SDHC_DATA7, 0x06000049) /* SDHC_DATA7 */
		>;
	};
};

 

What are the steps I should follow to configure it correctly? 

mmc0: switch to bus width 8 failed

 

Is QCVS PinMuxing Tool the right and sufficient solution for me to solve this problem?

0 Kudos
Reply
1 Solution
1,749 Views
zeroqruel
Contributor III

I solved the problem. In the RCW file, it was necessary to activate the function for emmc from the SPI_PCS pin settings.

zeroqruel_0-1747976922036.pngzeroqruel_0-1747976922036.png

 

SPI_PCS_BASE=2

View solution in original post

0 Kudos
Reply
1 Reply
1,750 Views
zeroqruel
Contributor III

I solved the problem. In the RCW file, it was necessary to activate the function for emmc from the SPI_PCS pin settings.

zeroqruel_0-1747976922036.pngzeroqruel_0-1747976922036.png

 

SPI_PCS_BASE=2

0 Kudos
Reply