LS1088A DDR Size Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1088A DDR Size Problem

跳至解决方案
2,948 次查看
TahaBenderli
Contributor I

Hello,

we are having a DDR4 size problem on LS1088a platform.  We have 4GB DDR4 on the board. When u-boot starts it is confirmed that board has 4GB DDR4. But when we checked on kernel with cat /proc/meminfo or free commands, it shows that RAM is 2GB.  Do you have any idea why are we having mismatch DDR size in u-boot and kernel ?

Attached photos you can see the differences.

 

freeddr4.jpgmeminfoddr.jpgubootddr4.jpg

0 项奖励
回复
1 解答
2,933 次查看
mcbridematt
Contributor III

The 2GB is being reserved for the DPAA2 MC memory. The best solution is to delete the "mcmemsize" variable from your U-Boot configuration which will reduce the total reservation down to 512MB.

在原帖中查看解决方案

2 回复数
2,934 次查看
mcbridematt
Contributor III

The 2GB is being reserved for the DPAA2 MC memory. The best solution is to delete the "mcmemsize" variable from your U-Boot configuration which will reduce the total reservation down to 512MB.

2,921 次查看
TahaBenderli
Contributor I

Thanks. I changed the value of the mcmemsize but it seems solution is deleting it. Now DDR size is 3.6 Gbytes.

0 项奖励
回复