LS1088A - Clocking

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,335件の閲覧回数
juergene
Contributor III

Hello community,

i found some inconsistence in the LS1088A RM.

The figure below shows that the LS1088A has a USBCLK-Input, but i can't find anything about that Input in the Datasheet. 

pastedImage_1.png

But the LS1088A Datasheet says: 

pastedImage_2.png

Does the LS1088A has such an USB-Clock-Input ?

Best regards,

Juergen

ラベル(1)
タグ(3)
1 解決策
2,142件の閲覧回数
Pavel
NXP Employee
NXP Employee

The LS1088a USB controllers are the same as LS1043a or LS1046a USB controllers. See the Section 3.13.4 of the LS1043 Datasheet:

USB 3.0 SSPHY needs a reference clock. There are two options for the reference clock: SYSCLK or DIFF_SYSCLK/DIFF_SYSCLK_B.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,143件の閲覧回数
Pavel
NXP Employee
NXP Employee

The LS1088a USB controllers are the same as LS1043a or LS1046a USB controllers. See the Section 3.13.4 of the LS1043 Datasheet:

USB 3.0 SSPHY needs a reference clock. There are two options for the reference clock: SYSCLK or DIFF_SYSCLK/DIFF_SYSCLK_B.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------