LS1046ardb NAND boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046ardb NAND boot

1,977件の閲覧回数
kzambrano
Contributor III

Is it possible to boot from NAND on this board? If so, could you kindly provide a summary of the procedures and tools required? Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,877件の閲覧回数
Pavel
NXP Employee
NXP Employee

The LS1046ARDB board does not support NAND booting.

The LS1046ARDB supports SD and QSPI boot source.

See the SW5 switch setting in the LS1046ARDB Reference Manual.

See also the Section 4.4.8.2 of NXP SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------