LS1046ardb NAND boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046ardb NAND boot

1,975 次查看
kzambrano
Contributor III

Is it possible to boot from NAND on this board? If so, could you kindly provide a summary of the procedures and tools required? Thanks.

标签 (1)
0 项奖励
回复
1 回复

1,875 次查看
Pavel
NXP Employee
NXP Employee

The LS1046ARDB board does not support NAND booting.

The LS1046ARDB supports SD and QSPI boot source.

See the SW5 switch setting in the LS1046ARDB Reference Manual.

See also the Section 4.4.8.2 of NXP SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------