LS1046ARDB networking issue with core-image-minimal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046ARDB networking issue with core-image-minimal

ソリューションへジャンプ
1,567件の閲覧回数
ashutoshharry
Contributor III

Hi @yipingwang 

 

Flashed all firmware generated by core-image-minimal from yocto and borad bootup good.

[Internet] ----- RGMII1(eth0) --*--  LS1046ARDB --*---(eth2)SGMII1 ----- LAN network

WAN eth0 got IP from my router as DHCP client.

on LAN eth2 i am running DHCP server so client on behind eth2 is getting IP address ,

but i am not able to ping from eth2 to eth1 or clients on eth2 cannot access internet,

so we need install any kernel or user level package to get networking stack working in this case?

NOTE: enable forwarding and disabled all iptables but same issue

thanks please help in this urgent case

 

0 件の賞賛
返信
1 解決策
1,560件の閲覧回数
ashutoshharry
Contributor III

@swati_gupta  please help in this case

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,561件の閲覧回数
ashutoshharry
Contributor III

@swati_gupta  please help in this case

0 件の賞賛
返信