LS1046ARDB networking issue with core-image-minimal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046ARDB networking issue with core-image-minimal

Jump to solution
1,552 Views
ashutoshharry
Contributor III

Hi @yipingwang 

 

Flashed all firmware generated by core-image-minimal from yocto and borad bootup good.

[Internet] ----- RGMII1(eth0) --*--  LS1046ARDB --*---(eth2)SGMII1 ----- LAN network

WAN eth0 got IP from my router as DHCP client.

on LAN eth2 i am running DHCP server so client on behind eth2 is getting IP address ,

but i am not able to ping from eth2 to eth1 or clients on eth2 cannot access internet,

so we need install any kernel or user level package to get networking stack working in this case?

NOTE: enable forwarding and disabled all iptables but same issue

thanks please help in this urgent case

 

0 Kudos
Reply
1 Solution
1,545 Views
ashutoshharry
Contributor III

@swati_gupta  please help in this case

View solution in original post

0 Kudos
Reply
1 Reply
1,546 Views
ashutoshharry
Contributor III

@swati_gupta  please help in this case

0 Kudos
Reply