LS1046ARDB is down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046ARDB is down

1,703 Views
michaelchen_nsb
Contributor II

My LS1046ARDB is down, D7(ASELLP) is always ON

At the very beginning, bank0 can boot successfully, and bank4 can't

So, I set the switch to boot from bank4(sw3[5] ==> 1), It doesn't work

and after I switch back(sw3[5] ==> 0), bank0 can't boot either

What can I do?

BTW, I never download the RCW for bank0 !

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,585 Views
Pavel
NXP Employee
NXP Employee

The LS1046ARDB board supports SD boot.

Use SD boot for restoring of the u-boot.

See the Table 47 and the Section 4.4.8.8 of NXP SDK 2.0-1703 documentation:

http://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply