LS1046A with IFC directly connected to NAND without CPLD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A with IFC directly connected to NAND without CPLD

349件の閲覧回数
sk48
Contributor I
Hi Team,
 
We are tyring to interface the NAND flash directly from IFC without CPLD interface. We are using the
uboot version 2018. The NAND is not being detected in the uboot. nand info in uboot shows empty. We think our custom board with LS1046A interfacing with NAND is kind of similar to LS1046AFRWY which doesn't have cpld interface.
 
Could you please advice us on how to proceed with this case.
 
Thanks.
 
Best Regards
SAI Kumar
タグ(4)
0 件の賞賛
返信
1 返信

294件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to LS1043ARDB hardware design and software configuration.

In dts file arch/arm/dts/fsl-ls1043a-rdb.dts, please refer to the following configuration.

&ifc {
status = "okay";
#address-cells = <2>;
#size-cells = <1>;
/* NOR, NAND Flashes and FPGA on board */
ranges = <0x0 0x0 0x0 0x60000000 0x08000000
0x1 0x0 0x0 0x7e800000 0x00010000
0x2 0x0 0x0 0x7fb00000 0x00000100>;

nor@0,0 {
compatible = "cfi-flash";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x0 0x0 0x8000000>;
bank-width = <2>;
device-width = <1>;
};

nand@1,0 {
compatible = "fsl,ifc-nand";
#address-cells = <1>;
#size-cells = <1>;
reg = <0x1 0x0 0x10000>;
};

In configs/ls1043ardb_defconfig, please configure the following configurations.

CONFIG_SYS_FLASH_CFI=y
CONFIG_MTD_RAW_NAND=y

Please refer to the following section in include/configs/ls1043ardb.h

#ifndef SPL_NO_IFC
#define CONFIG_NAND_FSL_IFC
#endif

#define CONFIG_SYS_NAND_BASE 0x7e800000
#define CONFIG_SYS_NAND_BASE_PHYS CONFIG_SYS_NAND_BASE

#define CONFIG_SYS_NAND_CSPR_EXT (0x0)
#define CONFIG_SYS_NAND_CSPR (CSPR_PHYS_ADDR(CONFIG_SYS_NAND_BASE_PHYS) \
| CSPR_PORT_SIZE_8 \
| CSPR_MSEL_NAND \
| CSPR_V)
#define CONFIG_SYS_NAND_AMASK IFC_AMASK(64*1024)
#define CONFIG_SYS_NAND_CSOR (CSOR_NAND_ECC_ENC_EN /* ECC on encode */ \
| CSOR_NAND_ECC_DEC_EN /* ECC on decode */ \
| CSOR_NAND_ECC_MODE_4 /* 4-bit ECC */ \
| CSOR_NAND_RAL_3 /* RAL = 3 Bytes */ \
| CSOR_NAND_PGS_2K /* Page Size = 2K */ \
| CSOR_NAND_SPRZ_64 /* Spare size = 64 */ \
| CSOR_NAND_PB(64)) /* 64 Pages Per Block */

#define CONFIG_SYS_NAND_ONFI_DETECTION

#define CONFIG_SYS_NAND_FTIM0 (FTIM0_NAND_TCCST(0x7) | \
FTIM0_NAND_TWP(0x18) | \
FTIM0_NAND_TWCHT(0x7) | \
FTIM0_NAND_TWH(0xa))
#define CONFIG_SYS_NAND_FTIM1 (FTIM1_NAND_TADLE(0x32) | \
FTIM1_NAND_TWBE(0x39) | \
FTIM1_NAND_TRR(0xe) | \
FTIM1_NAND_TRP(0x18))
#define CONFIG_SYS_NAND_FTIM2 (FTIM2_NAND_TRAD(0xf) | \
FTIM2_NAND_TREH(0xa) | \
FTIM2_NAND_TWHRE(0x1e))
#define CONFIG_SYS_NAND_FTIM3 0x0

#define CONFIG_SYS_NAND_BASE_LIST { CONFIG_SYS_NAND_BASE }
#define CONFIG_SYS_MAX_NAND_DEVICE 1
#define CONFIG_MTD_NAND_VERIFY_WRITE

#define CONFIG_SYS_NAND_BLOCK_SIZE (128 * 1024)

 

0 件の賞賛
返信