LS1046A package length

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A package length

1,672 Views
patrickgoh
Contributor I

Hi,

Is there a excel sheet for package length of LS1046ASE8Q1A?

Need this info for pin delay entry for board routing?

Labels (1)
0 Kudos
Reply
1 Reply

1,541 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

On the QorIQ processors the parallel signals (like DDR interface signals) are matched at pins. The output/input timings are specified at the pins too. For example you can see in the LS1046 data sheet statements like “The parameters are specified at the component pins” or “Available eye for data (MDQ), ECC (MECC), and data mask (MDM) outputs at the pin of the processor.” So if you need to match signal traces you should not take into account die-to-pin lengths in the LS1046A.
I think excel sheet for package lengthes of LS1046A is not public document. So if you definitely need for it you should create request to the technical support.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply