LS1046A fuse programming.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A fuse programming.

1,749 Views
Ingo-Roda
Contributor I

Hi there,

I have a rather simple question, but do not find a clear answer in any of the manuals.

So, how often can a fuse be blown?

As far as I understand, only once, permanently.

The document "LS1046A Datasheet Rev. 4.pdf" says in Table 6:

"5. Only six secure boot fuse programming events are permitted per lifetime of a device."

What does this mean in detail?

Thanks in advance,

Ingo

0 Kudos
Reply
3 Replies

1,713 Views
Ingo-Roda
Contributor I

Thanks, Oswalag.

Just to be 100% certain: a fuse can only be blown once, right!?!

Have a nice day, too,

Ingo

0 Kudos
Reply

1,693 Views
Oswalag
NXP TechSupport
NXP TechSupport

It is correct.

BR. 

 

0 Kudos
Reply

1,725 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

The reason for the "six" fuse programming are: 1 for testing (burn OTPMK/SRKH, etc), 2 for production (burn ITS and/or WP). 3 to 6 is for revoke keys form key list.
The more you program the fuse, there are more possibilities that you accidentally burn other fuse bit that cause corruption. Base on the above reason, you should not need to burn the fuse more than 6 times.

Have a nice day.

 

0 Kudos
Reply