LS1046A development board DPAA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A development board DPAA

跳至解决方案
2,984 次查看
bijan
Contributor I

Hello,

We are working with a Layerscape FRWY-LS1046A development board, using a Yocto build, and SDK version 2.0-1703.

Currently, we have IPSec set up and working but are seeing poor performance. We are investigating using DPAA and have seen some promising examples with ipsec-secgw in DPDK.

Are there any specific tools that allow for secure tunnels closer to wire speed and that support packet fragmentation? Is ipsec-secgw a path we should investigate?

Thank you.

0 项奖励
回复
1 解答
2,953 次查看
yipingwang
NXP TechSupport
NXP TechSupport

ipsec-secgw doesn't have fragmentation feature.

It can reach the line speed for 1442 large packets.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,954 次查看
yipingwang
NXP TechSupport
NXP TechSupport

ipsec-secgw doesn't have fragmentation feature.

It can reach the line speed for 1442 large packets.

0 项奖励
回复
2,670 次查看
arun_ayachith
Contributor I

In the latest DPDK versions 22+ I see, an option 

--reassemble NUM

Is it valid or not? 
I see the code also, present for the same. It uses, librte_ipsec does ip fragmentation and reassembly.

we see SEC error 0x20001b1a being received at times on [Tx or Rx path]. So when we try to run SSH from end-2-end it fails.

Normal ping passes.

even pings with higher packet -size like 1800/1900 also pass.

we are stuck with this problem over SSH/SCP not working. 

Any direction would be of great help to us in proceeding in the project.

Thanks, Arun Ayachith

0 项奖励
回复
2,921 次查看
bijan
Contributor I
Thank you.
0 项奖励
回复