LS1046A USB Controller VBUS requirements

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A USB Controller VBUS requirements

跳至解决方案
5,581 次查看
jlt1
Contributor I

Hi,

I'm currently designing a PCB using an LS1046A, and wish to use the USB controllers.

I'm trying to figure out how to connect the VBUS pins on the controllers.The devices I am communicating with do not require a VBUS connection, just the data lines. I also do not have a 5V supply currently on my PCB, so I would have to place down a supply just for this VBUS connection. It seems unusual that a 5V supply is required in addition to the 3V3 and 1V0 USB supplies.

I think that connection is required but I can't find much documentation on this. The datasheet doesn't give requirements for the VBUS pins. AN5252 Table 22 says that connection is compulsory and the pins have a voltage range of "0-5.25V", but does not give an estimated current draw.

The LS1046ARDB schematic appears to connect the USB_3 VBUS to USB_P2_PWR, but this net is not powered (pin C1 of U3 is tied low). Does this mean that the USB3 bus is non functional on LS1046ARDB?

Are the VBUS pins compulsory for operation of the USB busses? if so, how much current do they draw? And are there any sequencing requirements for this power supply?

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
5,495 次查看
ufedor
NXP Employee
NXP Employee

> Are the VBUS pins compulsory for operation of the USB busses?

Yes.

 

> if so, how much current do they draw?

The current is negligibly small.

 

> And are there any sequencing requirements for this power supply?

No.

 

> pin C1 of U3 is tied low

USB2_PWREN is controlled by U8.

在原帖中查看解决方案

7 回复数
4,198 次查看
jimmy_zhao
NXP Employee
NXP Employee

When USB is configured as a USB host, VBUS pin is not used. It is only used when USB is configured as USB device. Connect a 3.3V to VBUS should work even it is configured as a USB device. 

0 项奖励
回复
5,495 次查看
jlt1
Contributor I

Thanks very much for the prompt reply ufedor!

> USB2_PWREN is controlled by U8.

Oops, not sure how I missed that IC, sorry!

>The current is negligibly small.

Negligibly small being <5mA? Just asking to see if it is feasible to use an LDO from my input rail, without burning too much power.

0 项奖励
回复
5,495 次查看
ufedor
NXP Employee
NXP Employee

> Negligibly small being <5mA? 

<50uA

5,483 次查看
spoulin
Contributor I

Hi @ufedor 

Is it mandatory to feed that pin with 5V ? or 3.3V would be ok ?

What is the use of this pin for the LS1046 internally ?

What is the VIH of this pin ?

Thanks in advance !

0 项奖励
回复
5,452 次查看
ufedor
NXP Employee
NXP Employee

The nominal voltage for this pin is 5 V.

There is an internal comparator; if VBUS drops below about 4.4v, an over-current is signaled and the port is shut down.

0 项奖励
回复
5,435 次查看
spoulin
Contributor I

Thanks Ufedor, it is appreciated.

Regards !

Sylvain

0 项奖励
回复
5,496 次查看
ufedor
NXP Employee
NXP Employee

> Are the VBUS pins compulsory for operation of the USB busses?

Yes.

 

> if so, how much current do they draw?

The current is negligibly small.

 

> And are there any sequencing requirements for this power supply?

No.

 

> pin C1 of U3 is tied low

USB2_PWREN is controlled by U8.