LS1046A: PHY register R/W failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046A: PHY register R/W failed

3,674 次查看
yoshimorizumi
Contributor I

Hi,

I'm using linux-4.14.104 which is based on LSDK-19.03, on the LS1046ARDB.
I tried the following "mii-tool" command, for read/write phy register.

# mii-tool -vv eth0

However, the command returns "Invalid argument".

   Using SIOCGMIIPHY=0x8947
   SIOCGMIIPHY on 'eth0' failed: Invalid argument

I applied the attached patch, and fixed this issue.
If this patch is appropriate, could you apply to next LSDK release?

The following information is provided for your reference.

This patch is based on the following changes.
It supports only the "SIOCGMIIREG" operation.
https://source.codeaurora.org/external/qoriq/qoriq-components/linux/commit/?id=119d4a46b0d6fa82e6454... 

Similar changes are proposed in the following threads.
https://community.nxp.com/thread/366062   

标签 (1)
2 回复数

3,445 次查看
ufedor
NXP Employee
NXP Employee

The issue was escalated to the LSDK support.

0 项奖励
回复

3,445 次查看
1271792207
Contributor II

Where to find this LSDK support。 LSDK-18.09 also have this problem。

0 项奖励
回复